Hi,
we have Revision 2.0 of the Si now.
we laod the code by pcie,but it can not boot(situation same as 1.0 Si).
when the code is loaded completed,then write the start address to magic address. but the 6678 can't boot.
we moved PC pointer to start address by Emulator ,then it can boot(it's mean the code is ok)
My question is : if the Revision 2.0 of the Si can boot from PCIE not use EEPROM?
My PCIE boot configure as bellow(Please check it):
our device status register value:0x00015809
LENDIAN=1 System is operating in Little Endian mode
BOOT[2:0]=100 (PCI)
BOOT[8:5]=0000 32bit
BOOT[12:10]=011 100M
BOOT9,BOOT4,BOOT3Reserved =>0
PCIESSEN=1 1 = PCIe module enabled
PCIESSMODE[1:0]=01 PCIe in Legacy End-point mode (support for legacy INTx)
PACLKSEL=0 Selects CORECLK(P/N)
BR
wuxiao