Other Parts Discussed in Thread: TL16C750
Hi
I want to know the initialization of UART1 for polling tx/rx mode.
Awaiting for positive response.
initcode:
UART_SYSC =0X02;
while((UART_SYSS & 0X01) == 0X01);
UART_IER = 0x00;
UART_MDR1 = 0x7; /* mode select reset TL16C750*/ /*Disable (default state)*/
UART_LCR = UART_LCR_BKSE _A | UART_LCRVAL;
UART_DLL = 0;
UART_DLH = 0;
UART_LCR = UART_LCRVAL; //0X03
UART_MCR = UART_MCRVAL; //
UART_FCR = UART_FCRVAL; //0X01 | 0X02 | 0X03
UART_LCR = UART_LCR_BKSE_A | UART_LCRVAL;
UART_DLL = baud_divisor & 0xff;
UART_DLH = (baud_divisor >> 8) & 0xff;
UART_LCR = UART_LCRVAL;
UART_MDR1 = 0; /* /16 is proper to hit 115200 with 48MHz */
Please correct the initialization of code
Regards
Alex