Hi.
I can see "CCCCCC" message in DM814x EVM board, without nand code, with nand booting.
Which case shows "?#?#?#" message?
We made board with DM814x CPU, it set nand boot, no boot code in nand flash.
It shows "?#?#?#" message.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ken,
I think this is the problem with baudrate or uart clock frequency?
What is the oscilator frequency you are feeding to the device?
What frequency you are feeding to UART module?
Regards
AnilKumar
Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question. Thanks!
Do you mean sw register setttings or hw oscilator?
There is no code in nand flash. In that case, "CCC" message show after booting.
It means, it can not set baudrate settings with software.
Can you explain, which HW part checking needed in detail?
Hi Ken,
In case of DM814X EVM input oscillator frequency is 20MHz, I am asking what is the input frequency for your custom board?
Are you sure you are setting 115200 baurate in your "Tera Term" for UART console.
Regards
AnilKumar
Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question. Thanks!
I can see the "CCC" message with TI814x EVM board, "###" message with new board.
It is sure, 115200 baurate settings is correct.
Which TI814x CPU pin is needed 20Mhz? Would you say, pin number?
We use 32.768khz oscilator for TI814x CPU.
Hi Ken,
You can look at DM814X TRM http://www.ti.com/lit/ug/sprugz8a/sprugz8a.pdf (section "2.3.2 Clock Structure")
OSC0 is feeding 20MHz.
Regards
AnilKumar
Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question. Thanks!