This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXMDKPO8328 RS232 connection



Dear all,

We have received a request from our customer .

In case you had the same experience or in case you have the know-how to overcome this issue please share it with us :

"I have issue with the RS232 connection. Although I have successfully tested my serial port with hyperterminal (connecting TX RX ports), but the pulse oximetry PC application software shows that the device is not connected."

Thanks in advance,

Norbert

  • Hello Team,

    Do you have an update on this?


  • Hi Michael,



    First of all thanks for your response. Actually I am the "original" owner of the case, and now I want to add a few more details.

    We tried to do separate UART loopback test as following:

    1. used the "evm5515_EVM_BSL_revb\evm5515_v1\tests\uart" test code downloaded from Spectrum Digital site.

    2. Connected the UART cable's 2 and 3 pins together.

    3. Compiled the code without errors or warnings

    4. Run the debug succesfully

    5. Got following message

    EXBUSSEL = 5000
    01 Testing UART...

    Then nothing happened for a while.

    Assumingly it should gave at least some errors. But nothing was happen. So now I even do not know if the transmitting is happening or not.

    Thank you in advance
    Regards
    Davit