This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cache On/Off/Configure 'C' Code API BSL



I needed one of the above a few weeks ago and hunted these forums and the downloads and could never find one.  It appears it is no longer part of the BSL.

I wrote one and am giving it to the community so no one else needs to reinvent the wheel.  I didn't see an attachment mechanism so I pasted the code in place below.  This blog editor mangled it pretty badly and I had to do manual patchup, so if it doesn't compile, it is likely 1-2 chars of typos.

TI, you can do better.  As you can see, this isn't much code, but it does take TIME and TESTING to get a reliable package.  This one is.  I have been using it for several weeks and have turned cahce on/off/sizes and seen the measured code execution time effects.

TI, please consider including something like this in future BSL releases.

Thanks for considering it, Chris

 

Example usage:

      CACHE_Init_L2  ( CACHE_L2MODE_DISABLED ) ; // I am using all of L2 for my fast arrays
      CACHE_Init_L1P ( CACHE_L1MODE_32KB ) ;
      CACHE_Init_L1D ( CACHE_L1MODE_32KB ) ;

 

evmc6748_cache.h: (I followed the naming convention so it even looks like it belongs in the BSL!)

#ifndef EVMC6748_CACHE_H

#define EVMC6748_CACHE_H


typedef enum {

CACHE_L2MODE_DISABLED= 0 ,

CACHE_L2MODE_32KB = 1 ,

CACHE_L2MODE_64KB = 2 ,

CACHE_L2MODE_128KB = 3 ,

CACHE_L2MODE_256KB = 4 , // this is the max available on the 6748 as of March 2012

CACHE_L2MODE_MAX = 7

} Cache_L2mode_t;

typedef enum {
CACHE_L1MODE_DISABLED= 0 ,

CACHE_L1MODE_4KB = 1 ,

CACHE_L1MODE_8KB = 2 ,

CACHE_L1MODE_16KB = 3 ,

CACHE_L1MODE_32KB = 4 , // this is the max available on the 6748 as of March 2012

CACHE_L1MODE_MAX = 7

} Cache_L1mode_t;

#define CACHE_L2CFG ( (volatile uint32_t *) 0x01840000 )

#define CACHE_L1PCFG ( (volatile uint32_t *) 0x01840020 )

#define CACHE_L1DCFG ( (volatileuint32_t *) 0x01840040 )

voidCACHE_Init_L2 ( Cache_L2mode_tL2mode ) ;

extern voidCACHE_Init_L1P ( Cache_L1mode_tL1mode ) ;
extern voidCACHE_Init_L1D (  Cache_L1mode_tL1mode ) ;

#endif

evmc6748_cache.h:

#include <evmc6748.h>

#include <evmc6748_cache.h>

extern voidCACHE_Init_L2 ( Cache_L2mode_tL2mode )

{

*CACHE_L2CFG = L2mode ;

}

extern voidCACHE_Init_L1P ( Cache_L1mode_t L1mode )

{

*CACHE_L1PCFG = L1mode ;

}

extern voidCACHE_Init_L1D ( Cache_L1mode_t L1mode )

{

*CACHE_L1DCFG = L1mode ;

}

<end of code and post>