Other Parts Discussed in Thread: DM3725, DM3730, TPS65950
Porting to a new board omap dm3730 and tps65950 to omap dm3725 and tps65950.
config is the same for new kernel. Audio output Handsfree works on both boards.
alsamixer controls on kernel 3.0.8 does not show the following. Was this removed or do I have something set wrong?
These controls appear on the earlier working version.
name='ALC Attack Release Capture Switch'
name='ALC Attack Release Capture Volume'
name='ALC Max Min Capture Switch'
name='ALC Max Min Capture Volume'
name='ALC Wait Time Capture Switch'
name='ALC Wait Time Capture Volume'
Hardware is essentially the same as a previous version built with 2.6.33 kernel.
recording from mic creates a file that changes with the input but plays back as silence.
strange coding looks like a single bit changing at the signal rate. Sine wave input.
hex values; 808080808080808080808080808080807F7F7F7F7F7F7F7F7F7F7F7F7F7F7F7F80808080... repeating pattern that changes with amplitude and frequency
Any idea what I might try?
thanks