Other Parts Discussed in Thread: AM3715
Hi Everyone,
I recently want to debug audio driver using KITL. So I enabled kitl and debugger and built new NK.bin. In the Eboot, I selected boot device from LAN9115 and selected KITL (debug) device from LAN9115 also. Then NK image was successfully downloaded to the device and system run well. I could also run my application, play audio files, and set breakpoints. The problem is the following:
When I set a breakpoint, the system stops at where the breakpoint is set. If I press F5, the system continues to run without problem. However if I want to watch the value of some variables, such as i or status, I get "i CXX0017: Error: symbol "i" not found". The same thing for status. Variables i and status are local variables defined in a function.
Does anyone know what the problem could be and how to fix it?
The hardware is Mistral EVM REV G with AM3715 processor.
BSP is BSP_WINCE_ARM_A8_02_00_00 under WEC7.
Regards,
James