Other Parts Discussed in Thread: AM3703
Dear all,
i have been working on am3703 custom board with linux 2.6.32 kernel .
i am trying to integrate 4x4 keypad for my board,for that i want to use twl4030_keyboard.c default driver.
i have took my default board config file as board-omap3beagle.c file in that i have mapped single key in each button like this
board_keymap[] = {
KEY(2, 2, KEY_1),
KEY(3, 2, KEY_5),
KEY(4, 2, KEY_9),
KEY(5, 2, KEY_WAKEUP),
KEY(2, 3, KEY_3),
KEY(3, 3, KEY_7),
KEY(4, 3, KEY_ESC),
KEY(5, 3, KEY_POWER),
KEY(2, 4,KEY_0),
KEY(3, 4,KEY_4),
KEY(4, 4,KEY_8),
KEY(5, 4,KEY_BACKSPACE),
KEY(2, 5,KEY_2),
KEY(3, 5,KEY_6),
KEY(4, 5,KEY_ENTER),
KEY(5, 5,KEY_MENU)
};
and it's been working fine with default twl4030_keyboard.c driver.
now i want to integrate multiple functionality in each button,like
KEY(2, 4,KEY_0) // here 2 col,4 row i have assign function as KEY_0,now i want assign KEY_0 along with KEY_A,KEY_B,KEY_C
if i press 1st time i should get KEY_0, 2cd time i should get KEY_A, 3rd time press i should get KEY_B, 4th time i should get KEY_C
please suggest me how to integrate it?
matrix_keypad_build_keymap(const struct matrix_keymap_data *keymap_data,
unsigned int row_shift,
unsigned short *keymap, unsigned long *keybit)
{
int i;
for (i = 0; i < keymap_data->keymap_size; i++) {
unsigned int key = keymap_data->keymap[i];
unsigned int row = KEY_ROW(key);
unsigned int col = KEY_COL(key);
unsigned short code = KEY_VAL(key);
keymap[MATRIX_SCAN_CODE(row, col, row_shift)] = code;
__set_bit(code, keybit);
}
__clear_bit(KEY_RESERVED, keybit);
}
one more thing in the above function , what __set_bit(code,keybit); function do ? i didn't understand.
if i change code= KEY_VAL(key) to code =KEY_VAL(30) ( 30 means KEY_A value) then it's been effecting instead of KEY_0 KEY_A is coming.
please suggest me i have been struggling with this integratoin .
thanks in advance!!!!