I am using a simulink model of Audio and Video Pass-through example
from the demos of Target for TI C6000(MAtlab 2007a) for DM642 EVM
board. (Matlab 2007a and Code Composer Studio 3.1). When I downloaded
the (*.out) to the target board, then I get the distorted video which
splits into 4 image.Also the color information is also distorted.
Whereas, Video stabilization demo (with gray level output) works fine.
1. Is their an integration problem of Matlab with ccs3.1?
2. What are the appropriate setting which are required to run this
simulink model?