This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual channel streaming on DM368

Dear Support,

I have CMOS sensor connected to DM368 for IP camera application. Capture resolution will be 1080P. Is it possible to create 2 diffenret instant of encoder from single capture channel.

i.e. 1) Instant 1 will encode 1080P@30 in H.264

      2) instant 2 will encode 720P@30 in MPEG4.

After encode both channel will be streamed on network.

If YES then how can I do this? Is there any demo application in DVSDK?

Regards,

Dipen Patel