This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 clock input



Hi everyone.the Hyperlink and PCIE are not required in my project.Does that mean the Clock input for Hyperlink and PCIe will be like this?

  • That is correct.  The P pin should be connected to the core voltage and the N pin should be tied to ground through a 1K resistor.  Note that the if a clock is not provided to the PCIE subsystem the PCIESSEN configuration pin should be pulled low at the rising edge of RESETFULLz to ensure that the PCIE subsystem is disabled.