Other Parts Discussed in Thread: TMS320C6701
Dear all,
We have developed a kit using TMS320C6701 processor and is working well with XDS510JTAG emulator if the boot process is internal.
If we changed the boot process to external (8 bit ROM boot process), "the target is failed to connect" message is appering as soon as the CCS opened.
If anyone comes accross this problem or if anyone knows the cause of the problem, Kindly reply to this post.
It is noted that we are using 8 bit EEPROM connected to CE1 and planned to execute the code from that.
Kind Regards,
Harivikram T.S.