Hello All,
I have a custom DM8148 board. All seems running well, except for the LCD RGB interface. I am seeing the DE (VOUT[0]_AVID) signal, or something like it, on each of the bit6 pins (VOUT[0]_B_CB_C[6], VOUT[0]_G_Y_YC[6], and VOUT[0]_R_CR[6]).
This behavior is seen on two boards. Can anyone think of a reason for this behavior? The pads seem too spread out to be a board short between all 3 or 4 lines.
Could this have anything to do with the VPSS firmware and disabled PCI? I have PCI disabled in my kernel, and the PVR modules complain about the missing symbol when loaded:
pvrsrvkm: Unknown symbol pci_save_state (err 0)
pvrsrvkm: Unknown symbol pci_request_region (err 0)
pvrsrvkm: Unknown symbol pci_enable_device (err 0)
pvrsrvkm: Unknown symbol pci_choose_state (err 0)
pvrsrvkm: Unknown symbol pci_enable_msi_block (err 0)
pvrsrvkm: Unknown symbol pci_get_device (err 0)
pvrsrvkm: Unknown symbol pci_disable_msi (err 0)
pvrsrvkm: Unknown symbol pci_set_power_state (err 0)
pvrsrvkm: Unknown symbol pci_clear_master (err 0)
pvrsrvkm: Unknown symbol pci_restore_state (err 0)
pvrsrvkm: Unknown symbol pci_set_master (err 0)
pvrsrvkm: Unknown symbol pci_disable_device (err 0)
pvrsrvkm: Unknown symbol pci_release_region (err 0)
WARNING: Error inserting vpss (/lib/modules/2.6.37+/kernel/drivers/video/ti81xx/vpss/vpss.ko): Unknown symbol in module, or unknown parameter (see dmesg)
FATAL: Error inserting omaplfb (/lib/modules/2.6.37+/pvrsrvkm: Unknown symbol pci_save_state (err 0)
kernel/drivers/gpvrsrvkm: Unknown symbol pci_request_region (err 0)
pu/pvr/omaplfb.kpvrsrvkm: Unknown symbol pci_enable_device (err 0)
o): Unknown symbpvrsrvkm: Unknown symbol pci_choose_state (err 0)
ol in module, orpvrsrvkm: Unknown symbol pci_enable_msi_block (err 0)
unknown parametpvrsrvkm: Unknown symbol pci_get_device (err 0)
er (see dmesg)
pvrsrvkm: Unknown symbol pci_disable_msi (err 0)
pvrsrvkm: Unknown symbol pci_set_power_state (err 0)
pvrsrvkm: Unknown symbol pci_clear_master (err 0)
pvrsrvkm: Unknown symbol pci_restore_state (err 0)
pvrsrvkm: Unknown symbol pci_set_master (err 0)
pvrsrvkm: Unknown symbol pci_disable_device (err 0)
pvrsrvkm: Unknown symbol pci_release_region (err 0)
FATAL: Error inserting bufferclass_ti (/lib/modules/2.6.37+/kernel/drivers/gpu/pvr/bufferclass_ti.ko): Unknown symbol in module, or unknown parameter (see dmesg)