Dear All,
I'm working with TI8148EVM and SDK 5.03.01.15
Our test bed is based on a 1080p60 source (which is our custom DM8148-based board) that play dm816x_1080p_demo.264 demo stream provided with the SDK root file system.
On the other side I have TI8148EVM that takes this input (via TVP7002) and run capture_dei_encode.oms OMTB script, without problems.
Now I have two questions:
1) is it true that this script takes a 1080p60 input, encode it with h264@60fps?
2) if so:
a) how can I change the script to capture/encode h264@30fps? is just enough to run capture_dei_encode_30fps.oms, which sets frameSkipMask?
b) I don't understand how this platform can do this. In fact inside "4-ARM solutions in TI SITARA ARM9, CorteA8 family + Integra & DaVinci overview.pdf" that I take at techday in milan (21 nov 2011), there's explicitally written that this platform (DM8148@600MHz) cannot do encode @1080p60 but only @1080p30 max.
I'm not a video expert so maybe I'm missing something somewhere (h264 encoder settings that make this possible or video source that it's "easy" to encode even @60fps)
Any help or comment is welcome.
Best Regards,
Andrea