Other Parts Discussed in Thread: CDCE62005, CDCE72010
The C6678 EVB uses 2x CDCE62005 which has 5 differential output clocks each. I am intending to use 1x CDCE72010 which has 10 output clocks.
However, the CDCE62005 and CDCE72010 seems a bit different. CDCE72010 is a Ten Output High Performance Clock Synchronizer, Jitter Cleaner and Clock Distributor whereas CDCE62005 is a Five/Ten Output Clock Generator/ Jitter Cleaner With Integrated Dual VCOs.
Could I replace 2x CDCE62005 with 1x CDCE72010 just like that. My concern is that I may lose some functionality if I switch from CDCE62005 to CDCE72010 (such as the Integrate VCO in CDCE62005 which is not mentioned in CDCE72010).