Hello!
In accordance with OMAPL138 specification it is possible to use up to 512MBytes of DDR2 memory.
As I understand, 2 DDR2 chips must be used. I have been searching for appropriate configuration but have no success.
The problem is I can see only DDR2 chips with 15-bit row and 10-bit column addressing (x8 banks) which actually allows to have 256MByte (8-bit) memory (x2 chips).
But OMAPL138 has 14-bits row addressing. How can I get 512MByte configuration?
Thank you!