This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5 and C6Accel



Hello

Thanks, for me this answer solved my problem, but now i try to use an existing CCS5 ARM project and add C6Accel functionality to it. 

I followed the 

Initial configuration steps Users with no experience with XDCtools and Codec engine

from

http://processors.wiki.ti.com/index.php/C6Accel_ARM_user_Documentation

but have proplems to use the compiler.opt and the linker.cmd files in CCS.

Moreover i am confused because at this link they say that no .cfg configutation file is required whereas the C6Accel_Reference_guide.pdf in the DVSDK 04_03_00_06/c6accel_1_01_00_07/docs says that it is reqired (as far as i understand it correctly).

I added a .c file to my existing CCS5 project and tried to compile it with several combinations of configurations but without succes. I attach the .c file and it would be really nice if one could give me a helping hand.

Regards

Wendelin

2045.C6Accel.c.txt