This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building DSPLink for Integra



I'm attempting to build DSPLink for Integra so that I can use it with C6EZAccel.  The Integra is not listed in the platform options in the dsplinkcfg.pl Perl script.  Which of these options are the correct option for building on the Integra?  

 Welcome to DSP/BIOS(TM) Link Configuration Utility
------------------------------------------------------

!!DSPLINK will be configured for Build OS: LINUX!!

!!DSPLINK Directory : /home/n5ac/dsplink_linux_1_65_01_06/dsplink!!

=========================================================
Chosen configuration is as follows:

****************** ERROR !!! ***************************
Please provide a valid Platform!
Following platform are supported currently:
ID-->DAVINCI
DaVinci SoC - C64P DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->DAVINCIHD
DaVinciHD SoC - C64P DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->OMAP3530
OMAP3530 SoC - C64P DSP interfaced directly to ARM Cortex-A8
This platform does not support multi DSP scenario
ID-->OMAP2530
OMAP2530 SoC - C64P DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->LINUXPC
Linux Box (PC) with PCI based cards
This platform support multi DSP (PCI cards) architecture
ID-->DA8XX
DA8XX SoC - C674x DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->OMAPL1XX
OMAP-L1XX SoC - C674x DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->DM357
DM357 SoC - C64P DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->LEO
LEO SoC - C64P DSP interfaced directly to ARM11
This platform does not support multi DSP scenario
ID-->OMAPL138
OMAP-L138 SoC - C674x DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
ID-->DA850
DA850 SoC - C674x DSP interfaced directly to ARM9
This platform does not support multi DSP scenario
Provided:
Example: --platform=DAVINCI or --platform=<ID> or --help for all options

Would it be the OMAP3530 since it supports the Cortex_A8 or a DaVinci?

Steve
  • I'm going to try this, but I have no idea if it is correct:

    n5ac@N5AC-U11:~/dsplink_linux_1_65_01_06/dsplink/config/bin$ perl dsplinkcfg.pl --platform=OMAP3530 \
    --nodsp=1 --dspcfg_0=OMAP3530SHMEM --dspos_0=DSPBIOS5XX --gppos=OMAPLSP --comps=ponslrmc
    defined(%hash) is deprecated at dsplinkcfg.pl line 2069.
    (Maybe you should just omit the defined()?)
    defined(%hash) is deprecated at dsplinkcfg.pl line 2574.
    (Maybe you should just omit the defined()?)


    Welcome to DSP/BIOS(TM) Link Configuration Utility
    ------------------------------------------------------

    !!DSPLINK will be configured for Build OS: LINUX!!

    !!DSPLINK Directory : /home/n5ac/dsplink_linux_1_65_01_06/dsplink!!

    =========================================================
    Chosen configuration is as follows:

    Chosen platform:
    Identifier: OMAP3530
    Description: OMAP3530 SoC - C64P DSP interfaced directly to ARM Cortex-A8
    This platform does not support multi DSP scenario

    No of DSPs: 1

    Chosen combination for DSP0:
    Identifier : OMAP3530
    DSP Description : On-Chip DSP of OMAP 3530 SoC
    Physical Interface (PHY): OMAP3530SHMEM
    PHY Description : Shared Memory Physical Interface

    Chosen DSP OS for DSP0:
    Identifier: DSPBIOS5XX
    Description: DSP/BIOS (TM) Version 5.XX

    ****************** ADVICE !!! ***************************
    Binaries for DSP can be generated at preferred location
    For example: --dsp0_temp=/home/dsplink/dsp<#>/bin

    Chosen GPP OS for selected DSP(s):
    Identifier: OMAPLSP
    Description: OMAP LSP for OMAP2530 and OMAP3530

    ****************** ADVICE !!! ***************************
    Binaries for GPP can be generated at preferred location
    For example: --gpp_temp=/home/dsplink/gpp/bin

    Chosen Components for DSPLink:
    USE_PROC = 1
    USE_NOTIFY = 1
    USE_POOL = 1
    USE_MPCS = 1
    USE_MPLIST = 1
    USE_RINGIO = 1
    USE_MSGQ = 1
    USE_CHNL = 1

    ****************** ADVICE !!! ***************************
    To enable trace use option: --trace=1
    Provided:
    Assuming trace disable and continuing...

    ****************** ADVICE !!! ***************************
    To enable legacy support use option: --legacy=1
    Provided:
    Assuming legacy support disable and continuing...

    ****************** ADVICE !!! ***************************
    To enable DSP TSK mode select: --DspTskMode=1
    Provided:
    Assuming SWI mode enabled and continuing...
    =========================================================

    Configuration done successfully!!
    Generating CURRENTCFG.MK file...
    Generating multimake script...
    Generating CFG_system.c File...
    Generating GPP RTSC xdc file...
    Generating DSP RTSC xdc file...
    =========================================================
    Please edit the following files for toolchains, kernel sources, etc changes.
    GPP side distribution file: $DSPLINK/make/Linux/omap3530_2.6.mk
    GPP side distribution file: $DSPLINK/gpp/src/Rules.mk
    DSP side distribution file: $DSPLINK/make/DspBios/c64xxp_5.xx_linux.mk
    ==========================================================
    Users consuming DSPLINK as XDC package, Need to do the following.
    cd into the $(DSPLINK)/dsp directory and run:
    $(XDC_INSTALL_DIR)/xdc clean
    $(XDC_INSTALL_DIR)/xdc .interfaces
    cd into the $(DSPLINK)/gpp directory and run:
    $(XDC_INSTALL_DIR)/xdc clean
    $(XDC_INSTALL_DIR)/xdc .interfaces
    ==========================================================
    n5ac@N5AC-U11:~/dsplink_linux_1_65_01_06/dsplink/config/bin$
  • DSPLink does not support the DM8168/C6A8168:

    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/DSPLink/1_65_01_06/exports/dsplink_linux_1_65_01_06/dsplink_1_65_01_06_ReleaseNotes.html#Device_Support

    If you're trying to use c6ezaccel with that device then you will need the c6ezaccel 2.x code branch which is shipped inside the SDK according to here:

    http://processors.wiki.ti.com/index.php/C6EZAccel#Download

    The DM8168/C6A8168 EZSDK uses ezaccel 2.x in conjunction with syslink 2.x (not dsplink).  So the support you require would be part of syslink.

  • OK I expected to have to build them because of this comment in the "Introduction to C6Accel" document under "How to Install C6Accel":

    Assumption: The Build step assumes that the linux kernel, cmem and dsplink module have been pre-built. If the are
    not built users are expected to build those dependencies before building the C6accel package.

    I'll see if I can figure how to build it without these pieces -- thanks.

    Steve