This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please Read: OMAP4 Processors Forum Guidelines



Please note this Forum is now archived and available as Read-Only.

For further information, see this Forum thread.


This Read-Only Forum is intended as an hardware and software archive on TI OMAP4430, OMAP4460, OMAP4470, and companion processors (TWL604x, TWL603x). 

  • Search this forum for similar posts (use the search box above and to the right)
  • Search for answers at  TI OMAP wiki at http://omappedia.org

TI software releases on OMAP4 can be downloaded and installed as shown on omappedia.

OMAP4 TRMs, TRM addendums, DM, and Clock Tree Tool (CTT) are on TI website.

This Forum is NOT for questions about:  

  • Operating systems other than Linux and Android.  For Android in general refer to Android community mailing lists.
  • PandaBoard. Please post to the pandaboard@googlegroups.com.
  • Processors other than OMAP4430, OMAP4460, OMAP4470 and companion (TWL604x, TWL603x); for example, it is not for OMAP3430, OMAP3630.

Here are a few more guidelines for using the Forum:

  • Note that the Forum is only available as Read-Only
  • Please provide tags for your post with any relevant details or keywords to help the overall community (e.g. Android, kernel, OMAP44xx, USB etc)
  • If you are satisfied with the answer, please mark the thread as "Verified Answer"
  • Create separate posts for unrelated issues