This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAS+ Media Server Application/DM814x Power Consumtption



Hi Team

one of my design house customers is looking at designing a NAS + Media Sever Application and looking at use of DM8148 in the same. One of the key requirement of the application is less than 500mW power consumption in standby mode with Ethernet on.

Our power estimation spreadsheet provides it to be 755mA. Can you explain why is this so high as compared to other processors? Is 500mW a possibility in Standby mode?

 2577.DM814x_AM387x_PowerSpreadSheet_RevB.xls