Hi,
I have two queries regarding hardware cryptographic accelerators in DM8148, which are as follows
1 . Dose the DM814x Crypto API Driver (Linux drivers that provide access to the hardware cryptographic accelerators) supports rijndael (with block size of 192) ?.
2. Is there any documentation avilable for hardware cryptographic accelerators usage/programming ,for dm8148 platform?
Following are my setup details:-
sdk:- ezsdk 5_03_01_15
platform :- dm8148
patch:- NSS-Crypto-driver-software-beta-0.9.patch.gz applied