hi,
When we use the DM3730 to play 720p H.264 file, it doesn't work correct. The step we did is :
Hardware & software descript:
The BSP is BSP_WINCE_ARM_A8_01_02_00_Source.exe
The DVSDK is part of the BSP,Version is dvsdk_wince_01_11_00_02
The board is our's design, migration from OMAP3530.
The chip is DM3730CUSA, 800M
we use the WINCE's Media player to play the two fies:
MPEG4 file: davincieffect_mpeg4_aac_720p.mp4
H264 file: davincieffect_h264vid_mpeg1l3aud_d1ntsc_722kbps.avi
the problems descript:
When we uncheck the 720P option in the DVSDK, build the image ,it can play 480p H.264 file ,but can not paly 720p H.264 &720p MPGE4 files.
When we check the 720p option in the DVSDK, build the image, it can play 720p MPGE4 file, it can not play 480p h.264 file and 720p h.264 file. When play h.264 file, the Media palyer's progress bar stop at the begin piont, and the video window is black, while when stop play, there do have output information on the console.
Does the DM3730 Support H.264 under the Wince6 & how to solve the problem?