Other Parts Discussed in Thread: DM3730, OMAP3530
When we use the DM3730 to play the h.264
file on wince6 there meet some problems:
The software&hardware is :
1、
BSP used BSP_WINCE_ARM_A8_01_02_00_Source.exe
2、 DVSDK is part of BSP_WINCE_ARM_A8_01_02_00,the
version is dvsdk_wince_01_11_00_02
3、 The board was designed according to OMAP3530,
4、 The chip is TMS320DM3730CUSA 800M
5、 The tested media file is : davincieffect_mpeg4_aac_720p.mp4
& davincieffect_h264vid_mpeg1l3aud_d1ntsc_722kbps.avi
Problems Description
When we uncheck 720p option of the DVSDK, the
Built image can play the 480p h.264 file ,but cannot play the 720p
h.264&mpge 4 file.
When we select 720p option of DVSDK, The built
image can play 720p mpge4 file, but cannot play the 720p h.264 file & 480p
h.264 file. When use the media player play the 720p or 480p h.264 file , the
progress bar of the stop at the start point, and the video window keep black.
While when stop the player, the console
is still alive.
We do not sure that,Do the DM3730
support 720p decode on WinCe6, If it support, how can we solve this problem?
Thanks.