Hi TI,
What is the reason that C6EZ tool is removed from DM8168 EZSDK 5.03 ?
What problems will I face if I download C6accel and use it in DM8168 EZSDK 5.03 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
What is the reason that C6EZ tool is removed from DM8168 EZSDK 5.03 ?
What problems will I face if I download C6accel and use it in DM8168 EZSDK 5.03 ?
Hi,
You can still download and use C6Accel if you wish. Note that they have not been formally verified with EZSDK 5.03 but are expected to work as is.
Hi Siddharth,
C6accel was verified to be workable with previous versions.
Logically, C6accel should continue to be available in EZSDK 5.03.
Why C6accel has to be removed from EZSDK 5.03 ?
Hi,
The decision was strategic not to include C6Accel in the EZSDK. C6Accel usage will continue to be supported but we will no longer package it inside the EZSDK.
Hi Siddharth,
When I add a new C6accel kernel, it returns a status code of "-7".
Which source file contains the error definition of "-7" ?
How to debug this "-7" error ?
Thanks,
Mr Tan
Hi TI,
I have used the CE_DEBUG=2.
Attached is the error log.
Please see if you can see the problem.
Thanks,
Mr Tan