Other Parts Discussed in Thread: OMAP-L138
Hi,
If I'm using a 4-bit mode configuration, ports MMCSD0_D4-7 are unused. Should these just be left floating? or should they be pulled up?
Also, the shcematic checklist recommends 51K pullups on the MMCSD lines, but nothing of that nature is mentioned in neither the datasheet or the technical reference manual. Can the pull-ups be omitted? (I need all the space I can have)
Regards
Koteich