Other Parts Discussed in Thread: TWL6030
Hello,
Does someone had tested sd/mmc with nfs?
After tried latest mainline tree and linaro 3.1, I found sd card doesn't work
with nfs or usb fs, and it works well with mmc fs. However blaze board doesn't
have the problem.
It seems the issue is related to power supply.
For blaze, I can see there is an extra mmc0 interrupt num which should be handled by
twl6030.
root@localhost:/root> cat /proc/interrupts | grep mmc
CPU0 CPU1
91: 145 0 GIC mmc1
115: 145 0 GIC mmc0
384: 1 0 twl6030 mmc0
But for panda, only two mmc interrupt nums exist.
root@localhost:/root> cat /proc/interrupts |grep mmc
91: 13 GIC mmc1
115: 0 GIC mmc0
PS: From schemtic, I found USB phy and mmc share same VIO_1V8, is it has impact about the issue.
Thanks,