This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4430 ES2.3 HS + YouTobe + ISC 4.0.4. Don't play video.



I have such hardware: custom OMAP4430 ES2.3 HS board with 1Gb memory

Software: ICS 4.04 + kernel 3.0.21 + ducati-m3.bin .

magic number RPRC
header version 2
header size 1012
header data
49990f759143557f704cd6efdc040615 /home/a0212502/build/l27_ics/ducati_syslink/src/ti/examples/srvmgr/ti_platform_omap4430_core0/debug/test_omx_sysm3.xem3
4405180 2011-12-08 15:31:34.302867158 -0600
9f000000
043a17e2fef5b1d4354d26b59063eb95 /home/a0212502/build/l27_ics/ducati_mmlegacy/WTSD_DucatiMMSW/platform/base_image/out/app_m3/release/base_image_app_m3.xem3
59507586 2011-12-08 15:47:12.674407451 -0600
9f070000
version:
rpmsg: 1.00.09.44-1-g3a6df4a-dirty
core0: 1.00.09.44-1-g3a6df4a-dirty
xdctools_3_22_03_41
ipc_1_23_01_26
bios_6_32_01_38
cgtarm-4.9.0
core1: TI-MM-DUCATI_RLS.02.00.14.00_temp-dirty
xdctools_3_22_03_41
ipc_1_23_01_26
osal_1_21_01_08
bios_6_32_01_38
cgtarm-4.9.0
codec_engine_3_21_00_19
xdais_7_21_00_02
framework_components_3_21_01_26

section: 0, address: 0x80062000, size: 0x 558
resource table: 76
resource: 4, da: 0x9f000000, pa: 0x 0, len: 0x 8000, name: 0
resource: 4, da: 0x9f070000, pa: 0x 0, len: 0x 8000, name: 1
resource: 5, da: 0x 14211, pa: 0x 0, len: 0x 0, name: 0
resource: 5, da: 0x 328f69, pa: 0x 0, len: 0x 0, name: 1
resource: 6, da: 0x9f060000, pa: 0x 0, len: 0x 200, name: 0
resource: 6, da: 0x9f0d0000, pa: 0x 0, len: 0x 200, name: 1
resource: 1, da: 0x60000000, pa: 0x60000000, len: 0x10000000, name: IPU_TILER_MODE_0_1
resource: 1, da: 0x70000000, pa: 0x70000000, len: 0x 8000000, name: IPU_TILER_MODE_2
resource: 1, da: 0x78000000, pa: 0x78000000, len: 0x 8000000, name: IPU_TILER_MODE_3
resource: 1, da: 0xaa000000, pa: 0x4a000000, len: 0x 1000000, name: IPU_PERIPHERAL_L4CFG
resource: 1, da: 0xa8000000, pa: 0x48000000, len: 0x 1000000, name: IPU_PERIPHERAL_L4PER
resource: 1, da: 0xba000000, pa: 0x5a000000, len: 0x 1000000, name: IPU_IVAHD_CONFIG
resource: 1, da: 0xbb000000, pa: 0x5b000000, len: 0x 1000000, name: IPU_IVAHD_SL2
resource: 0, da: 0xa0000000, pa: 0xb3a00000, len: 0x 100000, name: IPU_MEM_IPC_VRING
resource: 0, da: 0x9f000000, pa: 0xb3b00000, len: 0x 100000, name: IPU_MEM_IPC_DATA
resource: 0, da: 0x 0, pa: 0xb3c00000, len: 0x 600000, name: IPU_MEM_TEXT
resource: 0, da: 0x80000000, pa: 0xb4300000, len: 0x 6000000, name: IPU_MEM_DATA
resource: 0, da: 0x88000000, pa: 0xba300000, len: 0x 5a00000, name: IPU_MEM_IOBUFS

section: 2, address: 0x 0, size: 0x 3c
section: 2, address: 0x 400, size: 0x 140
section: 2, address: 0x 4000, size: 0x 17bc4
section: 2, address: 0x80063cd0, size: 0x 200
section: 2, address: 0x9f0e0000, size: 0x 102f8
section: 2, address: 0x 0, size: 0x 3c
section: 2, address: 0x 800, size: 0x 140
section: 2, address: 0x 100000, size: 0x 49ac00
section: 2, address: 0x8047bd28, size: 0x a4044
section: 2, address: 0x8052595c, size: 0x 5674
section: 2, address: 0x8052efd0, size: 0x 200
section: 2, address: 0x9f0e0000, size: 0x 102f8
 

 After selecting video in Youtobe application I receive such output in console:

<6>rpmsg_omx rpmsg-omx1: local addr assigned: 0x401
rpmsg_omx rpmsg-omx1: local addr assigned: 0x401
<4>omap_hwmod: ipu: failed to hardreset
omap_hwmod: ipu: failed to hardreset
<6>omap-iommu omap-iommu.0: ducati: version 2.1
omap-iommu omap-iommu.0: ducati: version 2.1
<6>rpmsg_omx rpmsg8: conn rsp: status 0 addr 101
rpmsg_omx rpmsg8: conn rsp: status 0 addr 101

Video don't playing. How to resolve/debug this problem?