This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART



how can i deal with the UART in dsp kit  tmdsevm6670 i have read the datasheet and i wanna more info about it and how can i use it to transmit and receive data using CCS5

  • Hi Ahmed,

    Please, install the latest version of TI MCSDK, which is available below:

    http://software-dl.ti.com/sdoemb/sdoemb_public_sw/bios_mcsdk/latest/index_FDS.html

    Please, try running C6670 EVM platform test, which can be found at:


    <CCS_INSTALL>\pdk_C6670_1_0_0_XX\packages\ti\platform\evmc6670l\platform_test

    This platform test project, includes code which tests the UART connection on the C6670 EVM. For more details on how to run the test, please refer to the README file included in the project folder.

    The USB port (FTDI) on the C6670 EVM can be used as a serial port connection to the PC. More details can be found in C6670 technical reference manual:

    http://www.advantech.com/Support/TI-EVM/6670le_download3.aspx