Other Parts Discussed in Thread: AM3517
Hi,
We have a customer looking for MPEG1, Layer 2 audio encoders for the AM3517 that are optimized for the NEON co-processor. I pointed them to the FFMPEG encoders (ffenc_mp2 in particluar).
The customer doesn't believe these use NEON, can someone please clarify?
As I read this from (http://processors.wiki.ti.com/index.php/ARM_Multimedia_Users_Guide), I think they are NEON optimized:
“Open Source FFMpeg Codecs
FFmpeg is an open source project which provides a
cross platform multimedia solution.
- Free
audio and video decoder/encoder code licensed under GPLv2+ (GPLv3 license codecs can be build separately) - A comprehensive suite of standard compliant multimedia codecs
- Audio
- Video
- Image
- Speech
- Codec
software package
- Codec
libraries with standard C based API - Audio/Video
parsers that support popular multimedia content - Use
of SIMD/NEON instructions cortex-A8 neon architecture - Neon
provides 1.6x-2.5x performance on complex video codecs
Can someone clarify whether these codecs are NEON optimized? If they aren't, is there a source for MPEG1, Layer2 audio encoders that are? Thank you very much?