This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

arago do-fetch failed for u-boot-am33x from git



Hi,
        using my own .bb file I was trying to download u-boot-am33x from the following link :
    
  http://arago-project.org/git/projects/?p=u-boot-am33x.git;a=commit;h=d0e52e5b10ce05ddcee0a53bcdcbaeff70002d95

In the u-boot-am33x.bb i set the SRC_URL as follows :

  SRCREV = "d0e52e5b10ce05ddcee0a53bcdcbaeff70002d95"

  SRC_URI = "http://arago-project.org/git/projects/?p=u-boot-am33x.git;protocol=git;branch=master"

but when i run the bitbake for u-boot-am33x I am getting errors,showing do-fetch failed.
please refer below for error logs.Any suggestions would be helpful.
 
utc-arago@utc-arago-desktop:~/oe$
utc-arago@utc-arago-desktop:~/oe$ MACHINE=am335x-evm bitbake --buildfile=u-boot-am33x

Build Configuration:
BB_VERSION        = "1.10.2"
METADATA_BRANCH   = "master"
METADATA_REVISION = "da378da"
TARGET_ARCH       = "arm"
TARGET_OS         = "linux-gnueabi"
MACHINE           = "am335x-evm"
DISTRO            = "angstrom"
DISTRO_VERSION    = "2011.09"
TARGET_FPU        = "hard"

--2012-04-04 17:36:42--  http://arago-project.org/git/projects/?p=u-boot-am33x.git
Resolving arago-project.org... 184.73.161.183
Connecting to arago-project.org|184.73.161.183|:80... NOTE: Preparing runqueue
NOTE: Executing runqueue
connected.
HTTP request sent, awaiting response... NOTE: Running task 2 of 19 (ID: 9, /home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb, do_fetch)
NOTE: package u-boot-am33x-1.0-r12: task do_fetch: Started
NOTE: fetch http://arago-project.org/git/projects/?p=u-boot-am33x.git
200 OK
Length: unspecified [text/html]
Saving to: `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.8'

     0K .......... .......... .......                          28.0K=1.0s

2012-04-04 17:36:46 (28.0 KB/s) - `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.8' saved [28123]

--2012-04-04 17:36:46--  http://mirrors.openembedded.org//?p=u-boot-am33x.git
Resolving mirrors.openembedded.org... NOTE: fetch http://mirrors.openembedded.org//?p=u-boot-am33x.git
82.197.159.157
Connecting to mirrors.openembedded.org|82.197.159.157|:80... failed: Connection timed out.
Retrying.

--2012-04-04 17:37:09--  (try: 2)  http://mirrors.openembedded.org//?p=u-boot-am33x.git
Connecting to mirrors.openembedded.org|82.197.159.157|:80... failed: Connection timed out.
Retrying.

--2012-04-04 17:37:32--  (try: 3)  http://mirrors.openembedded.org//?p=u-boot-am33x.git
Connecting to mirrors.openembedded.org|82.197.159.157|:80... failed: Connection timed out.
Retrying.

--2012-04-04 17:37:56--  (try: 4)  http://mirrors.openembedded.org//?p=u-boot-am33x.git
Connecting to mirrors.openembedded.org|82.197.159.157|:80... failed: Connection timed out.
Retrying.

--2012-04-04 17:38:21--  (try: 5)  http://mirrors.openembedded.org//?p=u-boot-am33x.git
Connecting to mirrors.openembedded.org|82.197.159.157|:80... failed: Connection timed out.
Giving up.

--2012-04-04 17:38:42--  http://sources.openembedded.org//?p=u-boot-am33x.git
Resolving sources.openembedded.org... NOTE: fetch http://sources.openembedded.org//?p=u-boot-am33x.git
140.211.169.152
Connecting to sources.openembedded.org|140.211.169.152|:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 50 [text/plain]
Saving to: `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.9'

     0K                                                       100% 4.69M=0s

2012-04-04 17:38:44 (4.69 MB/s) - `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.9' saved [50/50]

--2012-04-04 17:38:44--  http://www.angstrom-distribution.org/unstable/sources/?p=u-boot-am33x.git
Resolving www.angstrom-distribution.org... 188.40.83.200
Connecting to www.angstrom-distribution.org|188.40.83.200|:80... NOTE: fetch http://www.angstrom-distribution.org/unstable/sources/?p=u-boot-am33x.git
connected.
HTTP request sent, awaiting response... 200 OK
Length: 52970 (52K) [text/html]
Saving to: `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.10'

     0K .......... .......... .......... .......... .......... 96% 8.12K 0s
    50K .                                                     100% 2.72K=6.8s

2012-04-04 17:38:52 (7.61 KB/s) - `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.10' saved [52970/52970]

--2012-04-04 17:38:52--  http://arago-project.org/files/sources/?p=u-boot-am33x.git
Resolving arago-project.org... 184.73.161.183
Connecting to arago-project.org|184.73.161.183|:80... NOTE: fetch http://arago-project.org/files/sources/?p=u-boot-am33x.git
connected.
HTTP request sent, awaiting response... 200 OK
Length: unspecified [text/html]
Saving to: `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.11'

     0K .......... ...                                         43.4K=0.3s

2012-04-04 17:38:53 (43.4 KB/s) - `/home/utc-arago/oe/downloads/index.html?p=u-boot-am33x.git.11' saved [13560]

ERROR: TaskFailed event exception, aborting
ERROR: Build of /home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb do_fetch failed
ERROR: Task 9 (/home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb, do_fetch) failed with exit code 1
ERROR: '/home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb' failed
NOTE: Task failed: Fetch failed: Unable to fetch URL http://arago-project.org/git/projects/?p=u-boot-am33x.git;a=commit;protocol=git;branch=master from any source.
NOTE: package u-boot-am33x-1.0-r12: task do_fetch: Failed
ERROR: TaskFailed event exception, aborting
ERROR: Build of /home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb do_fetch failed
ERROR: Task 9 (/home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb, do_fetch) failed with exit code 1
ERROR: '/home/utc-arago/oe/arago-oe-dev/recipes/U-bootbitbake/u-boot-am33x.bb' failed
utc-arago@utc-arago-desktop:~/oe$


 
  

  • Try setting your SRC_URI to use git://.......

    SRC_URI = "git://arago-project.org/git/projects/?p=u-boot-am33x.git;protocol=git;branch=master"

    Chase

  • Hi chase,

                    Thanks for the reply.Ya, I forgot to change the http protocol before. But after I changed it,

    its showing me different error that,the remote end hung up unexpectedly . I tried to clone it mannually,

    using 

               git clone git://arago-project.org/git/projects/?p=u-boot-am33x.git;protocol=git;branch=master

    but same above mentioned error is showing up.I do have similar kind of errors with two more recipe files:

    i) qt-patientcare_1.0.bb 

    ii) rt-tests_git.bb

        i)       with qt-patientcare_1.0.bb , where SRC_URI is set as below :

    BRANCH ?= "master"
    SRCREV = "ceb38cf2a0af923d79f64ccc4359c1ad401954ff"

    SRC_URI = "git://arago-project.org/git/projects/qt4-demos.git;protocol=git;branch=${BRANCH}"

               but after running the command  MACHINE=am335x-evm  bitbake  --buildfile=qt-patientcare_1.0

     ,i am getting below errors ::

    utc-arago@utc-arago-desktop:~/oe$ MACHINE=am335x-evm bitbake --buildfile=qt-patientcare_1.0

    Build Configuration:
    BB_VERSION        = "1.10.2"
    METADATA_BRANCH   = "master"
    METADATA_REVISION = "da378da"
    TARGET_ARCH       = "arm"
    TARGET_OS         = "linux-gnueabi"
    MACHINE           = "am335x-evm"
    DISTRO            = "angstrom"
    DISTRO_VERSION    = "2011.09"
    TARGET_FPU        = "hard"

    --2012-04-05 11:38:04--  http://www.angstrom-distribution.org/unstable/sources/git_arago-project.org.git.projects.qt4-demos.git_ceb38cf2a0af923d79f64ccc4359c1ad401954ff.tar.gz
    Resolving www.angstrom-distribution.org... NOTE: Preparing runqueue
    NOTE: Executing runqueue
    NOTE: Running task 2 of 19 (ID: 8, /home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb, do_fetch)
    NOTE: package qt-patientcare-1.0-r0.0: task do_fetch: Started
    NOTE: fetch http://www.angstrom-distribution.org/unstable/sources/git_arago-project.org.git.projects.qt4-demos.git_ceb38cf2a0af923d79f64ccc4359c1ad401954ff.tar.gz
    188.40.83.200
    Connecting to www.angstrom-distribution.org|188.40.83.200|:80... connected.
    HTTP request sent, awaiting response... 404 Not Found
    2012-04-05 11:38:06 ERROR 404: Not Found.

    From git://arago-project.org/git/projects/qt4-demos
     * branch            master     -> FETCH_HEAD
    NOTE: Creating tarball of git repository
    fatal: failed to unpack tree object ceb38cf2a0af923d79f64ccc4359c1ad401954ff
    ERROR: TaskFailed event exception, aborting
    ERROR: Build of /home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb do_fetch failed
    ERROR: Task 8 (/home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb, do_fetch) failed with exit code 1
    ERROR: '/home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb' failed
    NOTE: Task failed: Fetch failed: Unable to fetch URL git://arago-project.org/git/projects/qt4-demos.git;protocol=git;branch=master from any source.
    NOTE: package qt-patientcare-1.0-r0.0: task do_fetch: Failed
    ERROR: TaskFailed event exception, aborting
    ERROR: Build of /home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb do_fetch failed
    ERROR: Task 8 (/home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb, do_fetch) failed with exit code 1
    ERROR: '/home/utc-arago/oe/arago/recipes/ti/qt-patientcare_1.0.bb' failed
    utc-arago@utc-arago-desktop:~/oe$

    ii) with rt-tests_git.bb , where SRC_URI is set as below :

    SRCREV = "42ab9e7cd259fae674dc2b2aa2962caaf8f09409"

    PV = "0.51+${PR}+gitr${SRCREV}"

    SRC_URI = "git://git.kernel.org/pub/scm/linux/kernel/git/tglx/rt-tests;protocol=git"

                   but after running the command  MACHINE=am335x-evm  bitbake  --buildfile=rt-tests_git

     ,i am getting below errors :

    utc-arago@utc-arago-desktop:~/oe$ MACHINE=am335x-evm bitbake --buildfile=rt-tests_git

    Build Configuration:
    BB_VERSION        = "1.10.2"
    METADATA_BRANCH   = "master"
    METADATA_REVISION = "da378da"
    TARGET_ARCH       = "arm"
    TARGET_OS         = "linux-gnueabi"
    MACHINE           = "am335x-evm"
    DISTRO            = "angstrom"
    DISTRO_VERSION    = "2011.09"
    TARGET_FPU        = "hard"

    NOTE: Preparing runqueue
    NOTE: Executing runqueue
    NOTE: Running task 1 of 18 (ID: 10, /home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb, do_setscene)
    --2012-04-05 11:57:51--  http://www.angstrom-distribution.org/unstable/sources/git_git.kernel.org.pub.scm.linux.kernel.git.tglx.rt-tests_42ab9e7cd259fae674dc2b2aa2962caaf8f09409.tar.gz
    Resolving www.angstrom-distribution.org... NOTE: package rt-tests-0.51+r0+gitr42ab9e7cd259fae674dc2b2aa2962caaf8f09409-r0: task do_setscene: Started
    NOTE: package rt-tests-0.51+r0+gitr42ab9e7cd259fae674dc2b2aa2962caaf8f09409-r0: task do_setscene: Succeeded
    188.40.83.200
    Connecting to www.angstrom-distribution.org|188.40.83.200|:80... NOTE: Running task 2 of 18 (ID: 8, /home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb, do_fetch)
    connected.
    HTTP request sent, awaiting response... NOTE: package rt-tests-0.51+r0+gitr42ab9e7cd259fae674dc2b2aa2962caaf8f09409-r0: task do_fetch: Started
    NOTE: fetch http://www.angstrom-distribution.org/unstable/sources/git_git.kernel.org.pub.scm.linux.kernel.git.tglx.rt-tests_42ab9e7cd259fae674dc2b2aa2962caaf8f09409.tar.gz
    404 Not Found
    2012-04-05 11:57:52 ERROR 404: Not Found.

    fatal: The remote end hung up unexpectedly
    Cloning into /home/utc-arago/oe/downloads/git/git.kernel.org.pub.scm.linux.kernel.git.tglx.rt-tests...
    ERROR: TaskFailed event exception, aborting
    ERROR: Build of /home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb do_fetch failed
    ERROR: Task 8 (/home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb, do_fetch) failed with exit code 1
    ERROR: '/home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb' failed
    NOTE: Task failed: Fetch failed: Unable to fetch URL git://git.kernel.org/pub/scm/linux/kernel/git/tglx/rt-tests;protocol=git from any source.
    NOTE: package rt-tests-0.51+r0+gitr42ab9e7cd259fae674dc2b2aa2962caaf8f09409-r0: task do_fetch: Failed
    ERROR: TaskFailed event exception, aborting
    ERROR: Build of /home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb do_fetch failed
    ERROR: Task 8 (/home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb, do_fetch) failed with exit code 1
    ERROR: '/home/utc-arago/oe/arago-oe-dev/recipes/rt-tests/rt-tests_git.bb' failed
    utc-arago@utc-arago-desktop:~/oe$


       How to resolve this issue??? arago-tisdk-image is not getting build up because of these 2 packages.Any suggestions

    would be helpful from your side :)

    Thanks in advance,

    Surendra

  • Surendra,


    You may want to try your clone again.  Sometimes the arago server can get loaded with requests but I am able to do the clone myself this morning.

    Chase

  • Hi chase,

                    I tried it for several times but every time its showing me the same error.

    MACHINE=am335x-evm  bitbake  --buildfile=qt-patientcare_1.0

    MACHINE=am335x-evm  bitbake  --buildfile=rt-tests_git

                    Above 2 packages are not getting fetched from the source repository.The

    arago-tisdk-image is not getting build up because of this.One more query, why the

    SRC_URI is getting redirected to

    http://www.angstrom-distribution.org/unstable/sources/.............

                      I visited those links which shows the page doesnt exist.How to resolve

    this issue??Thanks for your patience reply :)

    Surendra

  • Surendra,

    I'm not sure about the --buildfile usage above.

    As for the SRC_URI redirection, that is the result of source mirroring.  The fetch will look to the mirrors first to see if the package exists there first, if not then it will fall back to cloning the repository.

    I have just done a fetch of both of these repositories with no issue.  Are you sure you have your GIT proxy setup correctly?

    Chase

  • Hi,

    why don't you try giving the command through command line, give the following command it works I have tried it works,

    /ti/am33x# git clone git://arago-project.org/git/projects/u-boot-am33x.git
    Cloning into u-boot-am33x...
    remote: Counting objects: 154797, done.
    remote: Compressing objects: 100% (28825/28825), done.

    .....

    Similarly you can clone other repositories, just change the the git path of the repo you want to clone.

    ex: git clone git://arago-project.org/git/projects/qt4-demos.git

    Thx,

    --Prabhakar Lad


  • Hi,

         Thanks for the reply.Chase, my intention was to create ipks using bitbake file.For other packages

    using the command MACHINE=am335x-evm  bitbake  --buildfile=<recipe name> , I was

    able to did the same.In this procedure the downloads folder gets populated with the package.tar.gz

    and corresponding package.tar.gz.md5. If i clone the qt-patientcare_1.0 using the git clone,

                  git  clone  git://arago-project.org/git/projects/qt4-demos.git;protocol=git;branch=master

    qt4-demos folder gets cloned.But there is no .tar.gz or .md5 for that folder.

                                 My query is that, how to work with that;i mean where to keep it (in downloads

    folder) and how to create .ipks out of it?? My final aim is to build the rtfs for arago-tisdk-image,

          MACHINE=am335x-evm  bitbake  --buildfile=arago-tisdk-image

    but in the middle of this building procedure its getting failed due to qt-patientcare_1.0.bb and rt-tests_git.bb.

    Prabhakar, rt-tests_git is not getting cloned using the git clone.How to resolve this issue for achieving build

    automation???

    Thanks,

    --Surendra

  • Hi,

    which branch are you trying to clone ? Can you post the link of it..

    Thx,

    --Prabhakar Lad

  • hi Prabhakar,

                          I have posted the rt-tests_git.bb file below.I need to create the .ipks using the .bb file.

    My query is that how come manual cloning is going to help me.For building rtfs I need these .ipk

    creations automatically to be done.How to resolve this issue??

    -------------------------------------------------- rt-tests_git.bb-----------------------------------------------------------

    DESCRIPTION = "Real-time tests, such as cyclictest, for real-time linux PREEMPT RT kernels"
    HOMEPAGE = "http://rt.wiki.kernel.org/index.php/Cyclictest"
    LICENSE = "GPL"
    PR = "r0"

    SRCREV = "42ab9e7cd259fae674dc2b2aa2962caaf8f09409"

    PV = "0.51+${PR}+gitr${SRCREV}"

    SRC_URI = "git://git.kernel.org/pub/scm/linux/kernel/git/tglx/rt-tests;protocol=git"

    S = "${WORKDIR}/git"

    # Limit to cyclictest only for non-real-time kernels.
    # EXTRA_OEMAKE = "cyclictest"

    TARGET_CC_ARCH += "${LDFLAGS}"

    do_install() {
      install -d ${D}${bindir}
      # any file that is executable by user and/or group
      for binary in `find . -perm /u+x,g+x -type f`
      do
        install -m 0755 $binary ${D}${bindir}
      done
    }

    ------------------------------------------------------------------------------------------------------------------------------

    thanks,

    --surendra

  • Surendra,

    I just realized that you are trying to build qt-patientcare.  That has been pulled in the qt4-demos repository.  the arago meta data was also updated in the next branch to remove this but has not yet been merged into master.  Please checkout the next branch of the arago repository because qt-patientcare has been removed there and rt-tests has been updated there.

    You can do this with

    git branch --track next origin/next

    git checkout next

    Chase

  • Hi chase,

                   Thanks.Yes,you were right.In next branch arago-tisdk-image is now getting build up.

    Right now I am trying to customize default arago-tisdk-image rtfs. I need to add some

    additional packages and need to delete unwanted ones.In arago/recipes/tasks recipe files

    by adding the .ipk package names I can do addition.But i am not sure about deletion process.

    I mean, I cross checked all 9 task recipe files contents (mentioned in arago-tisdk-image.bb )

    manually with installed-packages.txt (arago-tmp/deploy/glibc/images/am335x-evm/arago-tisdk-image-glibc-ipk-2011.09-am335x-evm-testlab/)

    and find out  additional 537 .ipk package names,about which i don't know how did they get

    incorporated in the installed-packages.txt.  Because they were not specifically mentioned in those

    9 task recipe files.

    examples:

    angstrom-version_1:2011.09-r7.6_am335x-evm.ipk
    arago-gpl-notice_1.0-r2.6_all.ipk
    bc_1.06-r2.6_armv7a.ipk
    binutils_2.20.1-r13.4-arago1.6_armv7a.ipk
    binutils-symlinks_2.20.1-r13.4-arago1.6_armv7a.ipk
    bluetooth-gui_1.0-r7+gitref5b7eb58c8125b826ca36d94c594f09f462b3ab.6_armv7a.ipk
    bonnie++_1.03c-r0.6_armv7a.ipk
    dbus_1.4.1-r20.0-arago3.6_armv7a.ipk
    dbus-x11_1.4.1-r20.0-arago3.6_armv7a.ipk
    debianutils_2.30-r2.6_armv7a.ipk
    directfb_1.4.11-r1.0-arago1.6_armv7a.ipk
    dt_17.07-r0.1.6_armv7a.ipk
    eggdbus_0.6-r0.6_armv7a.ipk
    gadget-init_1.0-r6.6_am335x-evm.ipk
    gconf_2.28.0-r2-arago1.6_armv7a.ipk
    gdk-pixbuf-loader-gif_2.20.1-r10.4.6_armv7a.ipk
    gdk-pixbuf-loader-jpeg_2.20.1-r10.4.6_armv7a.ipk
    gdk-pixbuf-loader-png_2.20.1-r10.4.6_armv7a.ipk
    gdk-pixbuf-loader-xpm_2.20.1-r10.4.6_armv7a.ipk
    gnome-keyring_2.28.2-r1.6_armv7a.ipk
    gnome-vfs_2.24.1-r3.6_armv7a.ipk
    gnome-vfs-plugin-file_2.24.1-r3.6_armv7a.ipk
    gst-ffmpeg_0.10.11-r1-arago1.6_armv7a.ipk
    gst-plugin-a52dec_0.10.16-r12.1-arago1.6_armv7a.ipk
    gst-plugin-adder_0.10.30-r12.0-arago1.6_armv7a.ipk
    gst-plugin-adpcmdec_0.10.20-r12.2-arago3.6_armv7a.ipk
    gst-plugin-adpcmenc_0.10.20-r12.2-arago3.6_armv7a.ipk.............etc

                  If I want to remove some of those out of 537 .ipk packages,hw am i suppose to do that???

    Any suggestion from your side would be helpful.Thanks in advance.

    --Surendra

  • Surendra,

    Those are likely pulled in as dependency packages the other packages.  Bitbake is good about that so that if you want to install a package that requires some other libraries (like perhaps libgcc) you don't have to call that out explicitly.  You can remove them from the file system using the package manager like http://processors.wiki.ti.com/index.php/AMSDK_File_System_Optimization/Customization.  But you need to be careful that you don't remove something that is a dependency of something you actually want to use.

    Using the -g option to bitbake.  i.e.:

    bitbake -g my-image

    Will give you a package-depend.dot file which you can look through to find out what packages are using a particular ipk and decide if you want to remove it.

    Chase

  • Hi Chase,
                          Thanks for your reply.Yes, using bitbake -g my-image three .dot files were generated,

    - pn-depends.dot, task-depends.dot and package-depends.dot.From the below link ,

                                  

            https://github.com/scottellis/oe-deptools

                       i got oey.py script file, using which I can find out the dependency tree for each packages (except library packages).

    I do have few queries which i pointed out below :

    1) My 1st query,what are the differences between these .dot files??

    2)Now I am facing problems with few recipe files which are not getting compiled (not getting converted into ipk packages)

       MACHINE=am335x-evm bitbake <recipe file name without .bb extension>

    i)    wvdial_1.60.bb (it shows Package libwvstreams was not found in the pkg-config search path.
                                     I tried to compile wvstreams.bb next ,but it  also failed)
    ii)   bluez-utils-3.36.bb
    iii)  ffmpeg_0.6.1.bb
    iv)  vim_7.2.bb (it shows two exact matches found.So I tried with gvim_7.2.bb and it got compiled.
                             Are both of them same??i mean gvim.bb downloads vim.tar.gz only)
    v)  glib-2.0_2.28.5.bb (it shows error "configure: error: Could not find a glib-compile-schemas in your PATH"
                                           do-configure failed. Although glib-2.0_2.24.1.bb is getting compiled)

         Right now I am working with master branch.Any idea how to resolve it???


    3) bluez-libs got compiled and following lists of ipks were created.

               i)   libbluetooth3_4.42-r1.1.6_armv7a.ipk
               ii)  libbluetooth-dbg_4.42-r1.1.6_armv7a.ipk
               iii) libbluetooth-dev_4.42-r1.1.6_armv7a.ipk
               iv) libbluetooth-doc_4.42-r1.1.6_armv7a.ipk
           I added libbluetooth3 in task-arago-tisdk-crypto.bb .It looks like below :


                RDEPENDS_${PN} = "\
                                  ${CRYPTO_SUPPORT} \
                                  ${WLAN} \
                                  ${BLUETOOTH} \
                                  libbluetooth3
                                  "
           but when i use MACHINE=am335x-evm bitbake arago-tisdk-image,its showing me error that,
         
    ERROR: '['/home/mirjisan/oe/arago/recipes/tasks/task-arago-tisdk-crypto.bb']' RDEPENDS/RRECOMMENDS or otherwise requires the runtime entity 'libbluetooth3' but it wasn't found in any PACKAGE or RPROVIDES variables
    Unknown Event: <bb.event.NoProvider instance at 0x137e53ac>
    NOTE: Runtime target 'libbluetooth3' is unbuildable, removing...
    Missing or unbuildable dependency chain was: ['libbluetooth3']
    NOTE: Runtime target 'task-arago-tisdk-crypto' is unbuildable, removing...
    Missing or unbuildable dependency chain was: ['task-arago-tisdk-crypto', 'libbluetooth3']
    ERROR: Required build target 'arago-tisdk-image' has no buildable providers.
    Missing or unbuildable dependency chain was: ['arago-tisdk-image', 'task-arago-tisdk-crypto', 'libbluetooth3']


                       Any suggestion,How to resolve these problems??? Thanks in advance :)


    With regards,

    Surendra
  • Surendra,

    I don't know all the differences in the .dot files but I use the package-depends.dot file to look at what dependencies are brought in by each package.

    For your other compile issues are you using the arago toolchain or codesourcery?  You should be using the Arago toolchain from inside of the SDK in the linux-devkit/bin directory.

    Lastly, for the bluez-libs package try just adding bluez-libs and not the libbluetooth3 package.

    Chase

  • Hi Chase,

                     for compilation i am using arago toolchain only.its arago-2011.09-armv7a-linux-gnueabi-sdk.

    export PATH=/opt/arago-2011.09/armv7a/bin:$PATH ,its working fine for other packages.Only above mentioned

    5 packages showing errors.Is there any other alternative way to do so??

    With regards,

    Surendra

  • Hi,

        I  was trying to add bridge-utils to my rootfs.bridge-utils_1.60.bb got compiled successfully and 5 .ipks were created.

    1.    bridge-utils_1.4-r0.6_armv7a.ipk
    2.    bridge-utils-doc_1.4-r0.6_armv7a.ipk
    3.    bridge-utils-dev_1.4-r0.6_armv7a.ipk
    4.    bridge-utils-dbg_1.4-r0.6_armv7a.ipk
    5.    bridge-utils-static_1.4-r0.6_armv7a.ipk

                                      I added both 1 and 5 in one of my task recipe file and rebuilt the rootfs. After successful completion its showing

    the package name in the installed packages list(arago-tmp/deploy/glibc/images/arago-tisdk-image-glibc-ipk-2011.09-am335x-evm-testlab/)

    but the command brctl is showing 0 bytes in arago-tmp/deploy/glibc/images/arago-tisdk-image-glibc-ipk-2011.09-am335x-evm.rootfs.tar.gz/usr/sbin.

    The same case with telnetd,tftp(inetutils added),tftpd,scp,ssh,httpd,ssh......etc etc.I am bit confused why this things happening??As per my understanding,

    for a specific package ,If any of the main ipk not added then it may show the corresponding executable binary size "ZERO".But in my case, apparently

    everything seems normal.Any suggestions would be useful to me.

    with regards,

    Suman Gupta