Other Parts Discussed in Thread: AM3517
Hi.
My customer evaluates the rotation and the resize function using AM3517EVM.
When it runs the video loopback program with 270 degrees rotation and resize,
the system freezing occur after few minutes of the running program.
[Evaluation conditions]
-EVM: TI AM3517EVM
-EZSDK: Linux v5.03.02 + Patch for 270 degrees rotation
-Input image(NTSC): 720x480
-Output resize image: 504x378
The following evaluation conditions could run the program without system freezing.
-EVM: TI AM3517EVM
-EZSDK: Linux v5.03.02 + Patch for 270 degrees rotation
-Input image(Fixed): 720x480
-Output resize image: 456x342
Can anyone advise as to the causes and solutions?
Thanks in advance for your helps.
Regards,
Kanae