Other Parts Discussed in Thread: AM3359
Hi
Can any of the Sitara processor series support for ONFI NAND Flash interface? Specifrically Am335x?
Best Regards
Feroz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM3359
Hi
Can any of the Sitara processor series support for ONFI NAND Flash interface? Specifrically Am335x?
Best Regards
Feroz
Danny,
I'm not working on AM335x at present. But ONFI is supported in AM335x for sure.
Hi Biser,
Thank you for your reply.
I supporse that BCH16 can support this page; 4096 and the spare area size; 224-bytes.
I refer to the following Wiki site.
processors.wiki.ti.com/.../Raw_NAND_ECC
If my understanding is wrong, please let me know.
As for SYSBOOT[9] setting; I will confirm it with my customer.
Best regards,
Kanae
Hi Biser,
Thank for your reply.
Let me make sure that the rom code requires BCH16
for the page/spare area size such as 4096/224.
Is this meant that Micron MT29F32G08CBACAWP can be used for AM335x
because the page size is "x8: 4320 bytes (4096 + 224 bytes)" ?
Also, do you know the actual results of Micron MT29F32G08CBACAWP with AM335x?
Regarding SYSBOOT[9]; my customer sets "0".
I supporse "Micron MT29F32G08CBACAWP" has satisfied the requirements of AM335x as you replied.
Please let me know the other check points to this issue.
Best regards,
Kanae
Hi Biser-san,
Thank you for your reply.
The method to check NAND compatibility with ONFI: http://processors.wiki.ti.com/index.php/Determining_compatibility_between_ROM_Bootloader_(RBL)_and_Raw_NAND_devices#ONFI
I understand that AM335x ROM Bootloader (RBL) supports booting from a NAND device which supports any one of versions in ONFI specifications.
To determine NAND device to boot, should the conditions other than the ONFI support be checked?
Best regards,
Daisuke