This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

raw capture with Interface VPIF on OMAP L138



Hello all,

I'd like to use the interface VPIF on OMAP L138 but I don't know how to start.

I'm developing code for the DSP using CCS v5.


I configure registers to use interface VPIF in "raw data capture mode".

The registers are configured :

CCD/CMOS datacapture mode: progressive, 8-bit/pixel

0x8120F704;             //C0CTRL                     C0CTRL:  FIELDFRAME=1, YCMUX=0, CAPMODE=1, CHANEN=0
0x00000404;             //C1CTRL                    
0x00000013;             //INTEN                         INTEN: ERROR=1, FRAME0=1
0x00000013;             //INTSET                       INTSET: ERROR=1, FRAME0=1
0x00000013;             //INTSTATCLR   
0x00000020;             //BYTES                        REQSIZE = 32 bytes
C0TLUMA;                 //0xC0000000              C0TLUMA = top of luma buffer in DDR
C0THANC;                //0x0000000F
0x00000000;            //C0BHANC
C0TVANC;                //0x0000000F
0x00FF01FF;            //CH0_SUBPIC_CFG
C0IMGOFFSET;        //0x00000200
C0HANCOFFSET;     //0x0000000F
C1TCHROMA;          //0x0000000F
C1THANC;                //0x0000000F
C1TVANC;                //0x0000000F
0x00FF01FF;            //CH1_SUBPIC_CFG
C1IMGOFFSET;        //0x0000000F
C1HANCOFFSET;    //0x0000000F

Any registers not listed have been zeroed. Ancillary data is not used.


I enable C0 and C1 at the end, after completing all other initialization.


C1CTRL: CHANEN=1

C0CTRL:CHANEN=1

I am now receiving interrupts from the VPIF in register INTSTAT bit 1 "Frame0"

My questions are :

- Where the data stored?


- which memory is used?


- I must configure memory?

Does anyone have any suggestions on how to proceed after initialisation?

Thanks in advance,

Fabien

PS : sorry for my bad English!  ^_^