This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 EMAC example – how can I increase the packet send & receive rates?



Hi,

I used the EMAC example (PA_emacExample_exampleProjec) as a basis to application that send & receive packets from the EVM board to an external PC.

The application is working fine, but the performance is very poor… the packet send & receive rates are very low (less than 100 packets per second).

 

I am getting this message: “No Tx free descriptor” although I increased the number of descriptors significantly.

 

I found that the problem is maybe related to the SGMII configuration. When I configure port 1 (Init_SGMII function) similar to the loopback configuration in the  EMAC example , the packets send rate is good (of course the packets are not arriving to the external PC).

 

What can be the cause of this performance degradation?

 

Thanks!

  • DO you have the setup in a local network. If you have a lot of traffic in the network, that might slow the performance.

    Thanks,

    Arun.

  • Hi,

    The C6678 EVM  is connected to 2 CPU through network switch, and all the packets/data in the network are sending from the EVM or to the EVM - but in very low rates.

    The performance is poor even if I’m disconnecting the network cable to the EVM (in transmit from EVM mode).

     

    I think that something in my configuration is wrong… but it’s based on the EMAC example (PA_emacExample_exampleProjec).

     

    I’m seeing the same behavior in the EMAC example:

    When I’m changing the MAX_NUM_PACKETS define to:

    #define                     MAX_NUM_PACKETS                         10000u

    and configure the SGMII (in “Init_SGMII” function) to:

    CSL_SGMII_disableMasterMode (macPortNum);

    // CSL_SGMII_enableLoopback (macPortNum);

     

    Thanks.