This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM6678LE Access FPGA registers

I'm trying to update some FPGA configuration registers. I've found the addresses for the registers in http://wfcache.advantech.com/support/TMDXEVM6678L_Technical_Reference_Manual_2V00.pdf

Is there something special I need to do before changing these values?  I've tried connecting with the probe, running the GEL file to initialize everything/map memory, and then changing the values via the memory browser for a quick test.  This doesn't seem to work.

I'm most interested in changing the clock source (SPI + 0x50), but for a sanity check I'm trying to control the debug LEDs (SPI + 0x8, bits 3-0).  For the SPI base address I'm using 0x20BF0000 as the base address (as defined in the tech reference manual).

I've also tried changing the LEDs via a program, and that didn't seem to work either:

    unsigned char mask[2] = {0xAA, 0x55};
    int i = 0;
    while (1)
    {
        Task_sleep(100);

        *(volatile unsigned char*)(CSL_SPI_BASE + 0x8) = mask[i];

        if (++i > 1) i=0;
    }

  • I've figured it out by looking at some code in the IBL.  I had to do some SPI protocol stuff.  Here's what I ended up with.  Now I have blinking LEDs!

    #define DEVICE_REG32_W(x,y)   *(volatile unsigned int *)(x)=(y)
    #define DEVICE_REG32_R(x)    (*(volatile unsigned int *)(x))
    #define FPGA_WRITE_REG_CMD(addr,byte)       (((addr & 0x7f) << 8) | (byte & 0xff))
    #define FPGA_ICS557_SEL_CTRL_REG    0x50 /* ICS 557 Clock Selection Control Register*/
    #define FPGA_LED_REG    0x8 /* ICS 557 Clock Selection Control Register*/
    #define DEVICE_SPI_BASE(x)          0x20bf0000u
    #define DEVICE_SPI_MOD_DIVIDER      6
    #define DEVICE_SPI_MAX_DIVIDER      0xff
    #define SPI_REG_SPIGCR0         0x00
    #define SPI_REG_SPIGCR1         0x04
    #define SPI_REG_SPIFLG          0x10
    #define SPI_REG_SPIPC0          0x14
    #define SPI_REG_SPIDAT0         0x38
    #define SPI_REG_SPIDAT1         0x3c
    #define SPI_REG_SPIBUF          0x40
    #define SPI_REG_SPIDELAY        0x48
    #define SPI_REG_SPIFMT(x)       (0x50 + ((x)*4))
    /* Register values */
    #define SPI_REG_VAL_SPIGCR0_RESET           0x0
    #define SPI_REG_VAL_SPIGCR0_ENABLE          0x1

    void setLEDs(unsigned char value)
    {
        /* Reset SPI */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);

        /* Release Reset */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_ENABLE);

        /* CS1, CLK, in and out are functional pins, FPGA uses SPI CS1 */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIPC0, 0xe02);

        /* prescale=7, char len=16 */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIFMT(0), 0x710);

        /* C2TDELAY=0x6, T2CDELAY=0x3 */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIDELAY, 0x6030000);

        /* Master mode, enable SPI */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR1, 0x01000003);

        /* Write ICS 557 Clock Selection Control Register in the FPGA */
        /* 1 : FPGA_ICS557_SEL s driven high */
        DEVICE_REG32_W(DEVICE_SPI_BASE(0) + SPI_REG_SPIDAT0,
                       FPGA_WRITE_REG_CMD(FPGA_LED_REG,value));
        chipDelay32(10000);
        /* Reset SPI */
        DEVICE_REG32_W (DEVICE_SPI_BASE(0) + SPI_REG_SPIGCR0, SPI_REG_VAL_SPIGCR0_RESET);
    }

    /*
     *  ======== taskFxn ========
     */
    Void taskFxn(UArg a0, UArg a1)
    {
        System_printf("enter taskFxn()\n");


        unsigned char mask[2] = {0xAA, 0x55};
        int i = 0;
        while (1)
        {
            Task_sleep(100);

            setLEDs(mask[i]);

            if (++i > 1) i=0;
        }

        System_printf("exit taskFxn()\n");
    }