This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe boot using Hello World example



Hi,

I have a 6670LE EVM running on Windows XP, MCDSK Ver. 2_00_05_17.  I'm trying to run the PCIe boot example for Hello World found in  tools\boot_loader\examples\pcie.  We have ported the Linux host loader to Windows XP but don't know if it works yet because we can't get the boards (EVM + EVMPCI) to enumerate (i.e. no indication that the boards are present is seen in Device Manager).  The doc for the PCIE Boot Example say to update the IBL.  Is this necessary since I haven't changed the IBL? 

Also, if I do need to update the IBL then the boot doc says perform steps (1) and (2) in evmc6670-instructions.txt.  Step (2) is "Programming the application on NAND or NOR flash".  What purpose does this serve since I'm trying to boot over PCIe?  I'm obviously missing something.

I believe I have the boot switches set correctly.  Any troubleshooting suggestions for determining why the boards won't enumerate?  I'm new at PCIe interfaces and I haven't found anything helpful in the postings.

Thanks.

Kevin