This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Generation tools



This project was created using a version of Code Generation tools that is not currently installed: 6.1.0.A11101 [C2000]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions.

How to download the Code Generation tools?How to configure in CCSv4?

  • Hi XIAOLONG LEE,

    You should be able to just select the version of the Code Generation tools that came with your CCSv4 installation.

    If you right click on the project and select build options, you should see a "Tools Settings" tab and under that "C2000".  If you click on C2000 you should see a place to select the version of the Code Generation tools that you want the project to use.

    Steve