Other Parts Discussed in Thread: TMS320C6678
I downloaded and installed Code Composer Studio version 5.2.0.00044 (for windows) for use with a TMS320C6678 evaluation module. It's an LE version, I believe, with a XDS560v2 emulator from Blackhawk. I've managed to get the examples running, as well as a sequential codebase I had lying around in C for CPUs. (I was surprised not to need to change a single line of code to get that working.)
However, I'm having trouble getting an OpenMP version working. In particular, the compiler version seems to be 7.3.1 and though I can add the -omp flag (it's on the project properties), there is no "omp.h" in the includes or anything else that I can see that hints at being an openmp include. And I get undefined symbol errors on the calls to get the number of threads ( omp_get_num_threads ) and the thread number ( omp_get_thread_num ) , plus the critical region pragma ( GOMP_critical_end , GOMP_critical_start , I believe ).
After looking through the forums here a bit I believe it's been announced that OpenMP support would only be offered in the upcoming 7.4.0 compiler (April 30 or so?).
Would anyone please confirm me whether my findings are correct and, if not, correct me? Also, if there is a pre-release library or something similar to enable openmp on my setup, how could I possibly get it?
Thank you for your attention.