Other Parts Discussed in Thread: TPS40400, PMP, TVP5158
Hi folks,
I am a beginner with the DaVinci and in this forum.
We are using a UdWorks DM8168 Rev. 05B platform with software DVRRDK_01_09_00_19.
Our development platform is a Ubuntu 10.04 running in Virtualbox.
At the moment we do the first steps with this device.
I compiled the Linux kernel and the dvr_rdk with success.
Now we want to load the kernel via Tftp and the root file systen via NFS.
Loading the kernel with Tftp works, the kernel starts up but getting the jffs2 rootfile system fails.
We have a NFS server (nfs-kernel-server) running on our host. The access to this server works fine.
I have tested this with an client from an external machine. The hosts firewall is turned off. The client has
access to the nfs root. But loading the jffs2 while startup up the DM8168 fails.
Do You have any idea what our prblem can be ?
Here is the log, the Uboot settings, hosts.deny, hosts.allow and exports:
UBOOT # boot
Connect speed 100M Full
Using DaVinci EMAC device
host 192.168.1.20 is alive
Connect speed 100M Full
Using DaVinci EMAC device
TFTP from server 192.168.1.20; our IP address is 192.168.1.10
Filename 'uImage_DM816X_DVR'.
Load address: 0x81000000
Loading: #################################################################
#################################################################
###############################
done
Bytes transferred = 2353616 (23e9d0 hex)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37
Created: 2012-02-07 7:43:56 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2353552 Bytes = 2.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Linux version 2.6.37 (root@ubuntu) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-
203) ) #1 Tue Feb 7 16:43:51 KST 2012
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: ti8168_dvr
vram size = 20971520 at 0x0
reserved size = 20971520 at 0x0
FB: Reserving 20971520 bytes SDRAM for VRAM
Memory policy: ECC disabled, Data cache writeback
OMAP chip is TI8168 1.1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 59396
Kernel command line: rootdelay=5 mem=254M console=ttyO2,115200n8 root=/dev/nfs r
w rootfstype=jffs2 nfsroot=192.168.1.20:/home/heb/tftproot ip=192.168.1.10:192.1
68.1.20:192.168.1.1:255.255.255.0::eth0:off vram=20M notifyk.vpssm3_sva=0xBFD000
00
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 234MB = 234MB total
Memory: 232276k/232276k available, 27820k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
vmalloc : 0xd0000000 - 0xf8000000 ( 640 MB)
lowmem : 0xc0000000 - 0xcfe00000 ( 254 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc0039000 ( 196 kB)
.text : 0xc0039000 - 0xc0476000 (4340 kB)
.data : 0xc0476000 - 0xc04b99c0 ( 271 kB)
SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:375
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
GPMC revision 6.0
Trying to install interrupt handler for IRQ368
Trying to install interrupt handler for IRQ369
Trying to install interrupt handler for IRQ370
Trying to install interrupt handler for IRQ371
Trying to install interrupt handler for IRQ372
Trying to install interrupt handler for IRQ373
Trying to install interrupt handler for IRQ374
Trying to install type control for IRQ375
Trying to set irq flags for IRQ375
OMAP clockevent source: GPTIMER1 at 27000000 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
omap_voltage_early_init: voltage driver support not added
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
3-wired eeprom init done. (H/W ver:5b)
_omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
_omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
registered ti816x_vpss device
registered TI816x on-chip HDMI device
registered ti816x_sr device
registered ti81xx_vidout device
pm_dbg_init: only OMAP3 supported
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
regulator: pmbus_vr: 800 <--> 1100 mV at 968 mV
regulator: tps40400 probe done.
omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
Advanced Linux Sound Architecture Driver Version 1.0.23.
Switching to clocksource gp timer
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
usb usb1: SerialNumber: musb-hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at d001e000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
musb-hdrc: kernel must blacklist external hubs
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
usb usb2: SerialNumber: musb-hdrc.1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at d0028800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
PMU: registered new PMU device of type 0
omap-iommu omap-iommu.0: ducati registered
omap-iommu omap-iommu.1: sys registered
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 453
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
console [ttyO2] enabled
brd: module loaded
loop: module loaded
ahci ahci.0: forcing PORTS_IMPL to 0x3
ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
scsi1 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
ata2: SATA max UDMA/133 irq_stat 0x00400040, connection status changed irq 16
omap2-nand driver initializing
NAND device: Maf ID: 0xec, Chip ID: 0xda (Samsung, )
erasesize: 0x20000, writesize: 2048, oobsize: 64
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000240000 : "U-Boot"
0x000000240000-0x000000280000 : "U-Boot Env"
0x000000280000-0x0000006c0000 : "Kernel"
0x0000006c0000-0x00000cee0000 : "File System"
0x00000cee0000-0x000010000000 : "Reserved"
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask fffffff8
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
rtc-ds1307 1-0068: rtc core: registered ds1337 as rtc0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc1
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.0.0)
OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
usb 1-1: new low speed USB device using musb-hdrc and address 2
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
notify_init : notify drivercreated for remote proc id 2 at physical Address 0x
bfd00000
usbcore: registered new interface driver snd-usb-audio
number of tvp5158 chips 4
chip address 59,chip address 5d,chip address 5b,chip address 5f,
tvp5158-audio.2-005c initial ok!
asoc: tvp5158-hifi <-> davinci-mcasp.0 mapping ok
asoc: SII9022a-hdmi-codec <-> davinci-mcasp.1 mapping ok
asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
asoc: HDMI-DAI-CODEC <-> hdmi-dai mapping ok
ALSA device list:
#0: TI81XX DVR
#1: TI81XX DVR (HDMI)
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
omap_voltage_late_init: Voltage driver support not added
Power Management for TI81XX.
smartreflex-ti816x: ti816x_sr_probe done!
rtc-ds1307 1-0068: setting system clock to 2012-04-05 12:51:22 UTC (1333630282)
usb 1-1: New USB device found, idVendor=046d, idProduct=c050
usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
usb 1-1: Product: USB-PS/2 Optical Mouse
usb 1-1: Manufacturer: Logitech
generic-usb 0003:046D:C050.0001: input: USB HID v1.10 Mouse [Logitech USB-PS/2 O
ptical Mouse] on usb-musb-hdrc.0-1/input0
davinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=1cc914)
IP-Config: Complete:
device=eth0, addr=192.168.1.10, mask=255.255.255.0, gw=192.168.1.1,
host=192.168.1.10, domain=, nis-domain=(none),
bootserver=192.168.1.20, rootserver=192.168.1.20, rootpath=
Waiting 5sec before mounting root device...
ata1: SATA link down (SStatus 0 SControl 300)
PHY: 0:01 - Link is Up - 100/Full
ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata2.15: Port Multiplier 1.2, 0x197b:0x3215 r0, 5 ports, feat 0x5/0xf
ata2.00: hard resetting link
ata2.00: SATA link down (SStatus 0 SControl 320)
ata2.01: hard resetting link
ata2.01: SATA link down (SStatus 0 SControl 320)
ata2.02: hard resetting link
ata2.02: SATA link up 3.0 Gbps (SStatus 123 SControl 320)
ata2.03: hard resetting link
ata2.03: SATA link down (SStatus 0 SControl 320)
ata2.04: hard resetting link
ata2.04: SATA link down (SStatus 0 SControl 320)
ata2.02: ATA-8: Hitachi HTS545050KTA300, BKFOC60M, max UDMA/133
ata2.02: 976773168 sectors, multi 0: LBA48 NCQ (depth 31/32)
ata2.02: configured for UDMA/133
ata2: EH complete
scsi 1:2:0:0: Direct-Access ATA Hitachi HTS54505 BKFO PQ: 0 ANSI: 5
sd 1:2:0:0: Attached scsi generic sg0 type 0
sd 1:2:0:0: [sda] 976773168 512-byte logical blocks: (500 GB/465 GiB)
sd 1:2:0:0: [sda] Write Protect is off
sd 1:2:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO
or FUA
sda: sda1
sd 1:2:0:0: [sda] Attached SCSI disk
VFS: Unable to mount root fs via NFS, trying floppy.
List of all partitions:
1f00 2304 mtdblock0 (driver?)
1f01 256 mtdblock1 (driver?)
1f02 4352 mtdblock2 (driver?)
1f03 204928 mtdblock3 (driver?)
1f04 50304 mtdblock4 (driver?)
0800 488386584 sda driver: sd
0801 488385560 sda1 00000000-0000-0000-0000-000000000sda1
No filesystem could mount root, tried: jffs2
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Backtrace:
[<c0047b90>] (dump_backtrace+0x0/0x110) from [<c0355060>] (dump_stack+0x18/0x1c)
r7:ce7d8000 r6:c006c540 r5:c002c7a4 r4:c04ba110
[<c0355048>] (dump_stack+0x0/0x1c) from [<c03550c4>] (panic+0x60/0x17c)
[<c0355064>] (panic+0x0/0x17c) from [<c0009254>] (mount_block_root+0x1e0/0x220)
r3:00000000 r2:00000020 r1:ce42bf58 r0:c04017cc
[<c0009074>] (mount_block_root+0x0/0x220) from [<c0009340>] (mount_root+0xac/0xc
c)
[<c0009294>] (mount_root+0x0/0xcc) from [<c00094d0>] (prepare_namespace+0x170/0x
1d4)
r4:c04b9a24
[<c0009360>] (prepare_namespace+0x0/0x1d4) from [<c0008784>] (kernel_init+0x114/
0x154)
r5:c0008670 r4:c04b99c0
[<c0008670>] (kernel_init+0x0/0x154) from [<c006c540>] (do_exit+0x0/0x5e4)
r5:c0008670 r4:00000000
The Uboot settings:
UBOOT # printenv
bootdelay=5
baudrate=115200
ipaddr=192.168.1.10
serverip=192.168.1.20
autoload=no
gatewayip=192.168.1.1
netmask=255.255.255.0
ntpserverip=192.168.1.151
timeoffset=32400
ethact=DaVinci EMAC
filesize=23E9D0
bootcmd 'ping 192.168.1.20; sleep 2; tftp 0x81000000 uImage_DM816X_DVR; bootm 0x81000000';
bootargs 'rootdelay=10 mem=254M console=ttyO2,115200n8 root=/dev/nfs rw rootfstype=jffs2 nfsroot=192.168.1.20:/home/heb/tftproot ip=192.168.1.10:192.168.1.20:192.168.1.1:255.255.255.0::eth0:off vram=20M notifyk.vpssm3_sva=0xBFD00000'
stdin=serial
stdout=serial
stderr=serial
ethaddr=44:aa:27:00:01:2e
eth1addr=44:aa:27:00:01:2f
hwver=00:5b
ver=U-Boot 2010.06 (Dec 08 2011 - 21:47:27)
My settings in exports:
/home/heb/tftproot 192.168.1.0/255.255.255.0(rw,insecure,async,no_subtree_check,no_root_squash)
/etc/hosts.deny:
portmap: ALL
mountd: ALL
nfsd: ALL
statd: ALL
lockd: ALL
rquotad: ALL
/etc/hosts.allow:
portmap: 192.168.1.0/255.255.255.0
mountd: 192.168.1.0/255.255.255.0
nfsd: 192.168.1.0/255.255.255.0
statd: 192.168.1.0/255.255.255.0
lockd: 192.168.1.0/255.255.255.0
rquotad: 192.168.1.0/255.255.255.0