Hi,
U disk USB connection to video source stored in the U disk, CPU utilization is relatively large, and may reach 90% when the video stream is relatively high at this time, the video freezes, and sometimes USB suddenly hang up, do not identifyre-insert the U disk, U disk can not be identified, and reboot the system recovery!
Please help to resolve as soon as possblie, Thanks!