Other Parts Discussed in Thread: SYSBIOS
Hi all:
I have a questionsabout using task module by sysbios,I
I create a empty RTSC project first, add a RTSC configruation File ,the source is:
var Task = xdc.useModule('ti.sysbios.knl.Task');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Main = xdc.useModule('xdc.runtime.Main');
var task0Params = new Task.Params();
task0Params.instance.name = "task0";
Program.global.task0 = Task.create("&taskfxn", task0Params);
add source file main.c
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
int main()
{
BIOS_start();
}
void taskfxn(UArg arg0,UArg arg1)
{
}
In this status,I can build the project correctly,but if I rename the main,c as main,.cpp because I want to use c++ on my project.
the error is
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_taskfxn D:\workspace1\mytask\Debug\configPkg\package\cfg\mytask_p674.o674
error: unresolved symbols remain
error: errors encountered during linking; "mytask.out" not built
Then the build wo't be successful.I wana konw wthat's the problem and how to fix it