Other Parts Discussed in Thread: SYSBIOS
hello,
I am a newer with c6748, I want to use the usb to communicate. I install BIOSPSP_01_30_01_Setup.exe and C6748_setupwin32_1_00_00_11.exe, But I only find one example :C:\C6748_dsp_1_00_00_11\rtfs_1_10_01_31\packages\ti\rtfs\examples\usbhostmsc\bios5\evm6748 for cc3 and for ccs4. And I use the CCS5.1. when I import the ccs4 project, when buile the project, it says cannot find " ti/biosusb/platforms/C6748/usb_evmInit.h". I need help! And if there is only one example of usb ? if yes ,can you give me some examples, Becase I am very anxious to use!
Thanks!