This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x-evm-sdk on beaglebone problem




U-Boot SPL 2011.09 (Feb 09 2012 - 15:38:59)
Texas Instruments Revision detection unimplemented
No AC power, disabling frequency switch
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2011.09 (Feb 09 2012 - 15:11:31)

I2C:   ready
DRAM:  256 MiB
WARNING: Caches not enabled
No daughter card present
NAND:  HW ECC Hamming Code selected
nand_get_flash_type: unknown NAND device: Manufacturer ID: 0x10, Chip ID: 0x10
No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0
*** Warning - readenv() failed, using default environment

Net:   cpsw
Hit any key to stop autoboot:  3  2  1  0
SD/MMC found on device 0
reading uEnv.txt

** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage

2922160 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Arago/3.1.0-psp04.06.00.03.sdk/a
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2922096 Bytes = 2.8 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.1.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Thu Feb 9 14:58:49 CST 2012
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 253724k/253724k available, 8420k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     DMA     : 0xffa00000 - 0xffe00000   (   4 MB)
[    0.000000]     vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0534000   (5296 kB)
[    0.000000]       .init : 0xc0534000 - 0xc056d000   ( 228 kB)
[    0.000000]       .data : 0xc056e000 - 0xc05c2d80   ( 340 kB)
[    0.000000]        .bss : 0xc05c2da4 - 0xc05fd320   ( 234 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz
[    0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[    0.000000] Console: colour dummy device 80x30
[    0.000253] Calibrating delay loop... 498.89 BogoMIPS (lpj=2494464)
[    0.058628] pid_max: default: 32768 minimum: 301
[    0.058790] Security Framework initialized
[    0.058912] Mount-cache hash table entries: 512
[    0.059362] CPU: Testing write buffer coherency: ok
[    0.064934] print_constraints: dummy:
[    0.065406] NET: Registered protocol family 16
[    0.065830] GPMC revision 6.0
[    0.068424] OMAP GPIO hardware version 0.1
[    0.071354] omap_l3_smx omap_l3_smx.0: couldn't find resource
[    0.071988] omap_mux_init: Add partition: #1: core, flags: 0
[    0.075901]  omap_i2c.1: alias fck already exists
[    0.077889]  omap2_mcspi.1: alias fck already exists
[    0.078180]  omap2_mcspi.2: alias fck already exists
[    0.108109] bio: create slab <bio-0> at 0
[    0.110992] SCSI subsystem initialized
[    0.113083] usbcore: registered new interface driver usbfs
[    0.113511] usbcore: registered new interface driver hub
[    0.113780] usbcore: registered new device driver usb
[    0.128789] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[    0.131449] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.132812] Switching to clocksource gp timer
[    0.138705] Switched to NOHz mode on CPU #0
[    0.153902] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.154133] musb-hdrc musb-hdrc.0: dma type: pio
[    0.155200] musb-hdrc musb-hdrc.0: USB OTG mode controller at d080a000 using PIO, IRQ 18
[    0.155411] musb-hdrc musb-hdrc.1: dma type: pio
[    0.156324] musb-hdrc musb-hdrc.1: USB OTG mode controller at d080c800 using PIO, IRQ 19
[    0.156814] NET: Registered protocol family 2
[    0.157052] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.157416] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.157640] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.157776] TCP: Hash tables configured (established 8192 bind 8192)
[    0.157792] TCP reno registered
[    0.157810] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.157842] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.158085] NET: Registered protocol family 1
[    0.158446] RPC: Registered named UNIX socket transport module.
[    0.158466] RPC: Registered udp transport module.
[    0.158479] RPC: Registered tcp transport module.
[    0.158491] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.158769] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.172819] VFS: Disk quotas dquot_6.5.2
[    0.172966] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.173747] JFFS2 version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    0.174149] msgmni has been set to 495
[    0.175124] io scheduler noop registered
[    0.175144] io scheduler deadline registered
[    0.175243] io scheduler cfq registered (default)
[    0.176355] Could not set LED4 to fully on
[    0.178408] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.180581] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.659987] console [ttyO0] enabled
[    0.664378] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.672236] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.680168] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.688038] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.695901] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.715591] brd: module loaded
[    0.725333] loop: module loaded
[    0.728865] i2c-core: driver [tsl2550] using legacy suspend method
[    0.735418] i2c-core: driver [tsl2550] using legacy resume method
[    0.741906] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.802863] No daughter card found
[    0.806495] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.821796] Board name: A335BONE
[    0.825208] Board version: 00A5
[    0.828508] The board is a AM335x Beaglebone.
[    0.833525]  omap_hsmmc.0: alias fck already exists
[    0.841749] mtdoops: mtd device (mtddev=name/number) must be supplied
[    0.848931] omap2-nand driver initializing
[    0.853581] OneNAND driver initializing
[    0.902879] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    0.909389] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    0.916784] davinci_mdio.0: probed
[    0.920369] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[    0.929199] CAN device driver interface
[    0.933257] CAN bus driver for Bosch D_CAN controller 1.0
[    0.939832] usbcore: registered new interface driver cdc_ether
[    0.946234] usbcore: registered new interface driver cdc_subset
[    0.952513] Initializing USB Mass Storage driver...
[    0.957911] usbcore: registered new interface driver usb-storage
[    0.964253] USB Mass Storage support registered.
[    0.969168] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.974856] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.982764] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.989936] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.997547] usb usb1: Product: MUSB HDRC host driver
[    1.002766] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd
[    1.008371] usb usb1: SerialNumber: musb-hdrc.1
[    1.014154] hub 1-0:1.0: USB hub found
[    1.018133] hub 1-0:1.0: 1 port detected
[    1.023665] mousedev: PS/2 mouse device common for all mice
[    1.030917] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[    1.037693] omap_rtc: already running
[    1.041843] i2c /dev entries driver
[    1.048636] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.055641] cpuidle: using governor ladder
[    1.060588] cpuidle: using governor menu
[    1.069282] usbcore: registered new interface driver usbhid
[    1.075227] usbhid: USB HID core driver
[    1.080254] usbcore: registered new interface driver snd-usb-audio
[    1.089170] ALSA device list:
[    1.092295]   No soundcards found.
[    1.095923] oprofile: hardware counters not available
[    1.101232] oprofile: using timer interrupt.
[    1.105771] nf_conntrack version 0.5.0 (3964 buckets, 15856 max)
[    1.112705] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.118486] TCP cubic registered
[    1.121887] NET: Registered protocol family 17
[    1.126596] can: controller area network core (rev 20090105 abi 8)
[    1.133221] NET: Registered protocol family 29
[    1.137896] can: raw protocol (rev 20090105)
[    1.142384] can: broadcast manager protocol (rev 20090105 t)
[    1.148410] Registering the dns_resolver key type
[    1.153467] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.161535] ThumbEE CPU extension supported.
[    1.166960] _regulator_get: mpu.0 supply mpu not found, using dummy regulator
[    1.174621] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=500000000 v=1100000)on vddmpu
[    1.183885] omap2_set_init_voltage: unable to set vdd_mpu
[    1.195186] Detected MACID=d4:94:a1:87:66:48
[    1.201600] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:03:30 UTC (946685010)
[    1.211060] Waiting for root device /dev/mmcblk0p2...
[    1.245003] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.256216] mmc0: new high speed SD card at address 1234
[    1.262652] mmcblk0: mmc0:1234 SA02G 1.83 GiB
[    1.271453]  mmcblk0:
[    1.323118] VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
[    1.330533] Please append a correct "root=" boot option; here are the available partitions:
[    1.339372] b300         1927168 mmcblk0  driver: mmcblk
[    1.344983] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
[    1.353873] Backtrace:
[    1.356493] [<c0017990>] (dump_backtrace+0x0/0x110) from [<c03e6c7c>] (dump_stack+0x18/0x1c)
[    1.365382]  r6:cf937000 r5:c055e9a4 r4:c05c3da0 r3:c058e250
[    1.371366] [<c03e6c64>] (dump_stack+0x0/0x1c) from [<c03e6cec>] (panic+0x6c/0x1a0)
[    1.379463] [<c03e6c80>] (panic+0x0/0x1a0) from [<c0534cb4>] (mount_block_root+0x184/0x228)
[    1.388260]  r3:c058e250 r2:00000000 r1:cf81bf58 r0:c04adf70
[    1.394242]  r7:00008000
[    1.396918] [<c0534b30>] (mount_block_root+0x0/0x228) from [<c0534f1c>] (mount_root+0xd8/0xe0)
[    1.405996] [<c0534e44>] (mount_root+0x0/0xe0) from [<c05350c4>] (prepare_namespace+0x1a0/0x1dc)
[    1.415246]  r4:c05c2e20
[    1.417920] [<c0534f24>] (prepare_namespace+0x0/0x1dc) from [<c053490c>] (kernel_init+0x124/0x130)
[    1.427352]  r5:c056ca28 r4:c056ca28
[    1.431142] [<c05347e8>] (kernel_init+0x0/0x130) from [<c004076c>] (do_exit+0x0/0x6a0)
[    1.439478]  r5:c05347e8 r4:00000000

 

 

then stopped,This is why?