Hi ,
I have modified supplied SDK mosaic demo to have following pipeline :
File H264 1080p60->DEC ->DEI ->SWMOSAIC->DISPLAY
|__ENC->File
This is working , Now I want to be able to change position and size of the displayed movie .
E.g move it and scale it down to some arbitrary size.
I am able to move the window by changing Mosaic Input and DEI Ouput parameters.
I have a problem in Scaling down the image , does EVM8168 supports this ?
Reading board spec I assume that hardware can do it , so what is the right way of doing it ?
I have tried to use both HD and MD Dei for this.
Thank You