This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 PCIE

Hi,

In our design,we use DM8148 and C6678.

 C6678 boot from PCIe by DM8148(DM8148 RC,C6678 EP),but the BAR is wrong:

 

ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xc6820000
ti81xx_pcie: INTx enabled legacy IRQ48
ti81xx_pcie: MSI info enabled msi_irq=49 msi_irq_num=32
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 9: assigned [mem 0x20000000-0x28ffffff pref]
pci 0000:00:00.0: BAR 8: assigned [mem 0x29000000-0x290fffff]
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x29000000-0x290fffff]
pci 0000:00:00.0: bridge window [mem 0x20000000-0x28ffffff pref]
PCI: enabling device 0000:00:00.0 (0140 -> 0143)
Finding the device....
Found TI device
TI device: vendor=0x0000104c, dev=0x0000b005, drv=0x00000000, irq=0x0030, bus=0xc2c7c200
Reading the BAR areas....
BAR0 start:0x0
BAR0 len:0x1000
BAR0 flag:0x40200
BAR1 start:0x10000000
BAR1 len:0x1000000
BAR1 flag:0x42208
BAR2 start:0x10000000
BAR2 len:0x2000000
BAR2 flag:0x42208
BAR3 start:0x12000000
BAR3 len:0x2000000
BAR3 flag:0x42208
Enabling the device....
pci 0000:01:00.0: Refused to change power state, currently in D3
PCI: Device 0000:01:00.0 not available because of resource collisions
Access PCIE application register .... RG zengxingyuan