This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need C6678 Optimized Image Segmentation/Region Labeling algorithm



Hello,

I currently have an application that takes 70ms to complete region labeling.  This is too long for my application.  The region is 1280x1280 and contains groups of zeros and ones.  I need to segment out the groups of ones into individually numbered groups. 

I am told this is a very basic image processing skill, does TI have an optimized library to do this?  I looked through the TI image processing library and did not see anything.

Please advise.

Thanks,
Brandy