This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nsf link create fail



Hi,

I am using rdk 02.00.00.23, I add nsf link into decode_display usecaes like as:

... -> ipclnVpss -> nsf -> dup -> swMs -> display

When I run my code the system happen an assert failed, message as following,

[m3vpss ]  13829: Assertion @ Line: 212 in links_m3vpss/nsf/nsfLink_drv.c: pObj->fvidHandleNsf != NULL : failed !!!

What does reason cause this happen? Does any restrict at nsf link?

Thanks,

Jacson