This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The Seagate 750GB SATA Hard Disk can not be recognized by DM8168



Dear all,

I use DVRRDK_02_00_00_23 as my code base and the chip version is P.G. 2.0. Unfortunately, the Seagate 750GB SATA hard disk can not be recognized by DM8168. But this is the one of Seagate SATA hard disks that can not be recognized, the others can work normally. It is a wonder that the Seagate 750GB SATA hard disk can be recognized by Silicon Image 3132(PCIE to SATA card). Can I say the DM8168 SATA interface will pick out the SATA hard disk? Please give me some explanations about this portion. Thanks a lot.

Please refer the Seagate 750GB hard disk information.

S/N : 5VP484CQ

ST3750528AS

P/N : 9SL153-515

Firmware : CC44

Date code : 10316

Site code : WU

B.R.

OC