According to the datasheet and Tech Ref manual
“AVS occurs continuously and in real time, helping to minimize power consumption in response to changing operating conditions.”
The core voltage clearly changes based on the SVT and HVT values (which I assume are hard-wired at manufacturing) but I have not seen it change dynamically.
Does SmartReflex actually adjust the core voltage dynamically? Under what conditions? If it adjusts on temperature, how is the temperature measured? If the system temperature is monitored, can this be used to adjust the core temperature to help with the issue of higher power at higher temperatures?
What is the meant by SmartReflex0 and SmartReflex1?
When are the SmartReflex IRQs asserted and how is the new voltage determined?
The Tech reference manual 3.2.3 references a "Power Management Software Guide". Where can I find this?
(We have reviewed the following AVS links)
http://processors.wiki.ti.com/index.php/DM816x_C6A816x_AM389x_AVS_Driver_Guide
http://processors.wiki.ti.com/index.php/DM816x_C6A816x_AM389x_AVS_FAQ