Other Parts Discussed in Thread: DP83848I, AM3352
Hi,
i'm using Micrel PHY KSZ9021RL on AM335x MPU, by using the AM335x EVM as reference design, here my connection:
| Am335x Pin | connect to | Micrel PHY KSZ9021RL |
| GMII1_TXCLK | GTX_CLK | |
| GMII1_TXD0 | TXD0 | |
| GMII1_TXD1 | TXD1 | |
| GMII1_TXD2 | TXD2 | |
| GMII1_TXD3 | TXD3 | |
| GMII1_TXEN | TXEN | |
| GMII1_RXCLK | RX_CLK | |
| GMII1_RXD0 | RXD0 | |
| GMII1_RXD1 | RXD1 | |
| GMII1_RXD2 | RXD2 | |
| GMII1_RXD3 | RXD3 | |
| GMII1_RXDV | RX_DV | |
| GMII1_MDIO_CLK | MDC | |
| GMII1_MDIO_DATA | MDIO | |
| GMII1_REFCLK | no connect | (none) |
| GMII1_COL | COL | |
| GMII1_CRS | CRS | |
| GMII1_RXERR | RX_ER | |
| (none) | no connect | INT_N |
since the AM335x EVM use Atheros AR8031 as PHY, i'm not sure my connections are correct. Are my connections correct?
Thanks & Regards
Keldy